This thread has been locked.
If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.
请教几个问题
1. poe控制芯片选择TPS2376-H,它后面接的DCDC电压输入范围应该是多少?是不是应该大于poe的最大输入电压57V?手册上figure14用的UCC3809最大输入电压是19V。
2. TI产品中PD大概分为两种,一种是PD only(TPS2376-H), 另一种为PD and DC/DC(TPS23758). 区别是不是在于,TPS23758需要接一个变压器,POE的输入和转换出来的电压(比如5V或12V)是隔离的,而TPS2376不隔离输入和输出的电源?
如果选择TPS23758可以不加变压器,只是输出5V或12V吗?节省一个DC/DC
非常感谢
HI
两者在电路上的差异主要在于TPS23758将DC/DC集成在控制芯片内,可以直接做成隔离方案。 而TPS2376后接的也可以是隔离方案,所以并不在于变压器。
如果你不可以不需要隔离,选择非隔离的方案也是可以的。
但是这类芯片的输入一般都是10V左右~57V.
感谢回答
不过还有第一个问题
TPS2376-H后面接的DCDC电压输入范围应该是多少?是不是应该能接受大于poe的最大输入电压57V?手册上figure14用的UCC3809最大输入电压是19V。
Hi
是的,需要接受输入端的最大电压57V.
UCC3809 VDD的最大电压是19V, 但是这个芯片设计的电源电路输入电压并非最大也19V, 大约19V的情况下做个regulation出来(三极管加稳压管)给电压到VDD即可。 输入母线电压可以远高于19V.