This thread has been locked.
If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.
1,原理图7673.lm3421-CST.pdf
2,如题:我参数也是这样设置,12.4K,和560K,但是我针对这2个电阻 无法调试参数,如我调试:12.4K变为15K,则就会变得关闭,因为这个属于OVP,电压超过1.24V。就保护了。
该如何设置电压到24V的方式?【设置高低电阻都无法解决电压稳定在Vled=24V】
参考计算方法:
1,OVP电压:在正常是1.24V以内,当如上设置15K时,VPO关闭,电压超过1.24,时1.35左右,但是无论怎么调都起不来,VLED电压要么是被保护时状态,要么是固定的33V左右【对GND是:57.5V左右】。
具体怎么设置限制Vled的高压,否则目前参数Vled=33V。Q1模式 我使用时60V,MOS管,否则会发烫。
2,另外电流设置是2.5A;
可看原理图参数:
3,IS设置悬空:
烦请尽快回复下,谢谢。
MOS Q1参数:MOS-N AON6244 60V +/-20V 85A 4.8mΩ/4.5V DFN5*6 SMT AOS
过流电阻:R6参数:CHIP RES 0.005Ω +/-1% 2W 2512 SMT