This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

LM3421: 无法限制升压,如Vinput=24V,Vled=24V。无法限制Vled是24V

Part Number: LM3421

1,原理图7673.lm3421-CST.pdf

2,如题:我参数也是这样设置,12.4K,和560K,但是我针对这2个电阻 无法调试参数,如我调试:12.4K变为15K,则就会变得关闭,因为这个属于OVP,电压超过1.24V。就保护了。

该如何设置电压到24V的方式?【设置高低电阻都无法解决电压稳定在Vled=24V】

参考计算方法:

  • 1,OVP电压:在正常是1.24V以内,当如上设置15K时,VPO关闭,电压超过1.24,时1.35左右,但是无论怎么调都起不来,VLED电压要么是被保护时状态,要么是固定的33V左右【对GND是:57.5V左右】。

    具体怎么设置限制Vled的高压,否则目前参数Vled=33V。Q1模式 我使用时60V,MOS管,否则会发烫。

    2,另外电流设置是2.5A;

    可看原理图参数:

    3,IS设置悬空:

    烦请尽快回复下,谢谢。

  • 空载时:Q1 mos管和R6过流电阻会很烫。当有负载时就不会。我出货给客户肯定要空载,若是发烫,肯定会坏。如何解决?

  • MOS Q1参数:MOS-N AON6244 60V +/-20V 85A 4.8mΩ/4.5V DFN5*6 SMT AOS

    过流电阻:R6参数:CHIP RES 0.005Ω +/-1% 2W 2512 SMT

  • Hi

        你选择的架构是buck-boost吗?  现在是OVP设计的问题吗? 将你的计算放上来看看?

x 出现错误。请重试或与管理员联系。