This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

BQ25792: 原理图设计

Part Number: BQ25792

hi  ,

BQ25792的线路我们应用在5V输入,输出12V3节电池充电,Icharge=1.2A,输出需要20W30W。线路如附件,麻烦帮忙check一下,有问题请指出,谢谢!

S21-BQ25792-DSD.pdf

线路中下面这个设置Input current limit地方,我不知道这样设置可不可以。

 

   因为输出需要20W,输入最大有25W,所以输入电流最大可能达到5A左右,所以分压设置到4.9V。但是我看datasheet上IIDPM好像最大是不是只能设置到3.3A