This thread has been locked.
If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.
在使用TPSM41625-2X-EVM评估板时,遇到输出电流上不去的问题,手册并未提及限流的相关问题。测试情况如下:
Vin = 5V,Vout = 0.9V。
1、当输出电流10A时,TPSM41625-2X-EVM电流输出只能到9.5A左右;
2、当输出电流大于10A时,TPSM41625-2X-EVM电流输出也只能到9.5A;
请问发生这样的情况时什么原因造成的?
备注:
测试Vin = 5V,Vout = 1.8V。TPSM41625-2X-EVM电流输出可以大于10A,但到19A左右就上不去了。