This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

TLV62569: 器件失效分析

Part Number: TLV62569


目前产品总量2W左右,返修出现电源IC TLV62569损坏的达0.5%,损坏芯片VIN和SW脚对地短路

产品工作环境为充电宝5V供电。

对产品进行了ESD测试,在电源VBUS端打接触8KV,空气15KV,没有损坏

浪涌测试,在±170V时,TLV62569损坏

电路图 和 SW 波形如下,目前测试发现的SW下冲最大达-2.5左右,芯片SW极限是-3V,不确定有没有影响