Part Number: UCC28782
在后续开关管电路单独测量没有问题后,尝试给UCC28782加电启动。但发现VDD已达到开启阈值,P13也正常在10us后才掉到13V,但RUN引脚无法随之拉高,从而无法正常产生PWM,VDD引脚并接电容一直保持充电又放电状态。请问是哪里没注意到吗?感觉datasheet里RUN引脚拉高条件已满足,但为何无法拉高呢?
This thread has been locked.
If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.
Hi
run输出高的前提是芯片正常工作,而仍然处于低说明芯片没有正常工作,VDD处于高低震荡即可说明,建议你再确认一下各个保护功能是否误动作,导致芯片不停重启?
当电路中只存在UCC28782的外围电路和SWS引脚处QS开关管的外围电路测试启动过程时,给QS漏极30V左右的电压,发现VDD只能维持在12.5V无法上升也没有高低震荡的情况,请问是由什么原因造成的呢?或者我应该怎么测试UCC28782的启动过程,并可以观察到PWML的输出呢。
对于之前触发保护的问题,测试条件为直接给主输入电容30V的直流电压,我通过数据表发现如果触发保护会出现PWML测试脉冲的出现,然而我在实际实验时并没有观察到这一现象。我想请问一下我的芯片外围电路的设计是否存在问题。或者可能是由于什么原因导致的呢。2330.原理图.pdf