This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

LM5175: 输入18V-36V输出28V,低压输入时,输出变高为30V

Part Number: LM5175


Dear TI:

             LM5175,电路设计输入18V-36V输出28V。

             空载输出时,输入为18V时,输出变高为30V,纹波如图;输入大于等于19V暂时没有此问题。

             请帮忙分析,谢谢~~~Power_Board_SCH_V1.02(211024).pdf