This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

TPS54302: 24V输入4.5V输出,电源纹波接到负载电源纹波有一段是50mV有一段25mV左右循环交替的是怎么回事

Part Number: TPS54302


整体波形如图,有一小截的25mV左右纹波,是符合手册纹波要求,但是出现尖的地方最高是50mV,循环周期性

取中间一段放大,左边是基本是标准的符合手册,右边是逐渐变成50mV的阶段

比较标准的频率400KZ,25mV左右

出现异常波形频率也异常,纹波最高能到50mV