This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

TPS54202: EN使能引脚问题

Part Number: TPS54202

如上图所示,R5本来需要贴105K,而贴成了1M,如果不考虑使用其中的调节欠压功能的话,这样会对芯片稳定或者性能造成影响吗?

目前我们有贴了5000多套,但是测试没有什么问题,输入电压24V,EN引脚按阻值分压应该是16V,实际测试接近7V。

看了规格书,EN引脚是0-7V之间,是内部钳位住了吗?这样长期使用会不会有什么影响?