Part Number: TPS74401
我用TPS74401芯片实现1.0V电源,输入是1.35V,bias接3.3V,EN脚通过10K上拉到3.3V,R1是1.13K,R2是4.53K结果发现输出不是1V而是1.35V,很奇怪为什么输出等于输入呢,
另外一路TPS74401芯片实现1.2V电源,输入是1.5V,bias接3.3V,EN脚通过10K上拉到3.3V,R1是2.49K,R2是4.99K结果发现输出不是1.2V而是1.5V,很奇怪为什么输出等于输入呢
This thread has been locked.
If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.
Part Number: TPS74401
我用TPS74401芯片实现1.0V电源,输入是1.35V,bias接3.3V,EN脚通过10K上拉到3.3V,R1是1.13K,R2是4.53K结果发现输出不是1V而是1.35V,很奇怪为什么输出等于输入呢,
另外一路TPS74401芯片实现1.2V电源,输入是1.5V,bias接3.3V,EN脚通过10K上拉到3.3V,R1是2.49K,R2是4.99K结果发现输出不是1.2V而是1.5V,很奇怪为什么输出等于输入呢
Hi
有正常的板子吗? 还是说做了很多板子有4片异常,其他正常?
有没有确认一下layout是否有异常,LDO应用相对简单,看看layout上是否有短路的现象?