This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

TPS74401: 电源输出始终等于电源输入,为什么呢

Part Number: TPS74401

我用TPS74401芯片实现1.0V电源,输入是1.35V,bias接3.3V,EN脚通过10K上拉到3.3V,R1是1.13K,R2是4.53K结果发现输出不是1V而是1.35V,很奇怪为什么输出等于输入呢,

另外一路TPS74401芯片实现1.2V电源,输入是1.5V,bias接3.3V,EN脚通过10K上拉到3.3V,R1是2.49K,R2是4.99K结果发现输出不是1.2V而是1.5V,很奇怪为什么输出等于输入呢