Part Number: TPS2660
TPS2660 Enable时,OUT端没有接负载所以没有电流,量测IMON电压发现会有50mV电压
TPS2660 disable时 ,量测IMON电压不会有50mV电压
TPS2660 的IMON电阻 是接到RTN ,但探棒是接GND
请问为何会有50mV的电压?
This thread has been locked.
If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.
Part Number: TPS2660
TPS2660 Enable时,OUT端没有接负载所以没有电流,量测IMON电压发现会有50mV电压
TPS2660 disable时 ,量测IMON电压不会有50mV电压
TPS2660 的IMON电阻 是接到RTN ,但探棒是接GND
请问为何会有50mV的电压?
下面第一张图是OUT端电流为100mA时, IMON 电阻用15.8K量测出来的波形 ,
OUT端电流为100mA时, IMON电压应该是123mV,但因为IMON电压量变化范围是0-300mV,
所以计算出来的电流变动很大
第二张图是加上10UF电容后量测出来的IMON波形
虽然仍有杂讯但IMON电压变化范围是108 -140mV
IMON电压比较接近123mV
请问
1.规格书有写到IMON是accuracy±8.5%,但规格书没有些到要加电容
所以没加电容时IMON电压量变化范围是0-300mV是正确的吗?
2.我要达到accuracy±8.5%, , 电容要加到多大
3.如果我要用RC电路,R跟C要用多大


Imon 会输出定电流,OUT端流经1A电流
Imon 会输出78.2uA电流 , 利用Rmon
就会产生电压 , 电压可以接到MCU用来判断电流
如果不加电容当OUT端是小电流时(如100mA)Imon的NOISE会很大
当OUT端是2A时NOISE就很小
因为规格书没有写要加电容
所以要请问一下当OUT端是小电流时(如100mA)Imon的NOISE会很大是正常的吗?
HI
noise很大可能和layout有很大关系。
Rmon靠近Imon, 到MCU的走线避免尽量避免noise干扰,可以在MCU端增加一个50~100ohm电阻看看效果,如果加电容的,尽量小一点,小于1000pF.(具体效果要对比IMON脚波形,和MCU输入端波形)