This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

LM5060: 設計詢問

Part Number: LM5060

你好

目前設計考慮使用LM5060,作為前級電路保護。

目前設計
電壓輸入為28V , over-voltage :30V   ,under-voltage:26V

電流: 15A ,max Current: 25A  ,minimum current :6A

請問建議設定與mosfet 選用,謝謝