This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

TPS650864: 电源管理芯片解惑

Part Number: TPS650864
Other Parts Discussed in Thread: TIDA-01393

问题一:对参考设计TIDA-01393的疑问:1. 参考设计中将BUCK1输出的5V电压接到PIN57(V5ANA),内部的Load switch开启,输出LDO5P0 。 LDO5P0又接到PIN38(DRV5V_1_6),及BUCK1的DRV电路输入端。 2. 如此设计形成一个环路,BUCK1输出5V,经过内部导通MOS(按手册导通电阻最大1Ω),接到BUCK1的输入DRV端。 对于BUCK电路,这样似乎不合理, 故存有疑惑,请协助解答。谢谢!  PS;具体请参照附件PMIC_TPS6508641设计说明

问题二:目前有个项目使用贵司的电源管理芯片TPS6508641RSKT,在调试中发现输出电压有drop的现象。具体请参照附件TPS6508641调试信息PMIC_TPS6508641设计说明(1).pptxTPS6508641调试信息.pptTPS6508641_SCH.pdf