This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

UCC28782: At 100Vdc input, the VDD gets 18V from the secondary winding, but the switch tube does not get PWM signal

Part Number: UCC28782
  •  The design objective  :input:90-265V,output:0-6A,20V
  • When the circuit works at 325VDC input and output 0-6A, the circuit normally outputs 20V and the simulation of the circuit is normal.

  • At 100Vdc input, When it operates at 10mA, the circuit works normally.But when it operate from 10mA to 3A,the circuit fails.The graph is follow: