- The design objective :input:90-265V,output:0-6A,20V
- When the circuit works at 325VDC input and output 0-6A, the circuit normally outputs 20V and the simulation of the circuit is normal.
- At 100Vdc input, When it operates at 10mA, the circuit works normally.But when it operate from 10mA to 3A,the circuit fails.The graph is follow:



就是官网提供的这个