Part Number: TPS40200
Other Parts Discussed in Thread: LMR16030,

这个电路,效率只有44%,我调了频率,调成100khz,把D1摘掉,现在效率68%,我的期望是80%,请问大神我该怎么调
This thread has been locked.
If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.
Hi
D1是必须去掉的,另外影响频率的因素有,选择尽量小Qg, Rdson的MOS, 以及饱和电流足够并且尽量低DCR的功率电感。
另外你的反馈已经补偿(FB/COMP)电路设计也建议参考datasheet来做。
如果希望效率尽量靠一些,可以选择同步芯片来做,例如LMR16030, 效率可以做到90%左右。电路可以直接借助webench仿真获得,相对TPS40200设计起来要简单得多。