This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

LM5160A: TIDA-00199 用于三相逆变器的宽输入隔离型 IGBT 栅极驱动 Fly-Buck 电源 - 参考设计

Part Number: LM5160A
Other Parts Discussed in Thread: TIDA-00199

在测试搭建的TIDA-00199电路当中,变压器二次侧四路23V输出的电压以及电流是可以稳定输出的,即功率是满足要求的;

但当搭建连接后端电路时,15V/-8的输出是不稳定的,此时变压器输出端主绕组测(5,6引脚)输出端电压只有8V左右;原边输出正常为10.6V;

搭建电路时只搭建了一路15V/-8V输出电路进行测试;芯片以及变压器都用的是原理图中的器件;