Other Parts Discussed in Thread: TIDA-00199
在测试搭建的TIDA-00199电路当中,变压器二次侧四路23V输出的电压以及电流是可以稳定输出的,即功率是满足要求的;
但当搭建连接后端电路时,15V/-8的输出是不稳定的,此时变压器输出端主绕组测(5,6引脚)输出端电压只有8V左右;原边输出正常为10.6V;
搭建电路时只搭建了一路15V/-8V输出电路进行测试;芯片以及变压器都用的是原理图中的器件;
This thread has been locked.
If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.
在测试搭建的TIDA-00199电路当中,变压器二次侧四路23V输出的电压以及电流是可以稳定输出的,即功率是满足要求的;
但当搭建连接后端电路时,15V/-8的输出是不稳定的,此时变压器输出端主绕组测(5,6引脚)输出端电压只有8V左右;原边输出正常为10.6V;
搭建电路时只搭建了一路15V/-8V输出电路进行测试;芯片以及变压器都用的是原理图中的器件;
Hi
变压器是找到对应厂商的变压器型号吗? 还是按照你现有规格自己设计的变压器?
Hi
不太明白你的意思,四路23V满载没有问题,但是后面又说,带载就会异常?
如果是带载输出电压偏低, 轻载正常吗?
其次我觉得变压器有些不对。
变压器用的就是设计推荐的型号,没有改变变压器;我计算了一下带负载能力,按照原理图中的设计,输出端带负载能力只有15V/0.01A,负载能力没有到达设计中提到的15V/0.1A
Hi
也就是带0.01A正常? 但是带到0.1A就异常偏低吗?
除了确认变压器外,就是要注意功率回路尽量小,因为这个也可能影响芯片的带载能力。