This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

LM5050-2: ORing电路选型

Part Number: LM5050-2
Other Parts Discussed in Thread: LM5050-1, , TPS2412

TI工程师好:

1,53.5V 30A电路需搭建ORing电路,选用LM5050-1和LM5050-2有什么应用上的区别吗?从官网的QA看到,LM5050-1可能存在漏电流回路,目前我们偏向选型LM5050-2。另外,不太理解nFGD引脚设计应对什么场合,FET TEST MOED检测,如果带了载进入了这个模式,把MOS管会迅速发热;但是如果是空载,检测不到IN和OUT引脚的电压也没有什么意义。这个引脚我们计划直接悬空处理

2,LM5050-2应用里面,选型建议使用Logic level MOS,不太理解这个指的是什么MOS,是否可以理解为GATE引脚驱动电压阈值较低?

3,12V 13A的电路也需要新设计ORing电路,正在选型芯片。LM5050-2和TPS2412两个方案在12V回路上应用有什么优劣吗?目前我们偏向基于LM5050-2去设计。

  • HI

       LM5050-1和LM5050-2的主要差别在于nFGD的控制,  这个主要是正侧MOS  DS压差的指示脚, 具体你可以看一下LM5050-2  datasheet第12页的说明.

       如果你不用到这个功能,实际上你选择LM5050-1也是可以的,选用LM5050-2不用这个功能也行。