This thread has been locked.
If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.
LM2577: 4节氢镍电池输入(4.8v),升压至8V(实际输出为8.6V)。电路按照Datasheet手册中经典用法设计电路。负载为两个小的直流电机(6V,150ma),以及其他数字电路。总体电流大概在800MA左右。
一开始使用100UH电磁屏蔽电感,实验加载负载后电感发热厉害,导致电感屏蔽罩烧裂。
最后换成工字电感100UH,在启动电机后,电感同样发热厉害,最后把外面的胶带都烧化,此时电流大概为900MA~1000MA. 数据手册也看了好几遍,也没有找到合适的解决方案。
请专家帮忙。
附上电路图:
开关电源一般使用功率电感,电感会发热主要由于其直流感抗DCR,乘以电流的平方后所产生的热量。因些,需要选用饱和电流足够大,DCR较小的功率电感以减小损耗及发热量。
Hi
此二级管的选型要求是尽量低VF的快速恢复的肖特基二极管,电流要求平均电流至少大于最大输出电流,峰值电流大于电感的峰值电流,在你的应用中至少应该选择1A以上的二极管,但是IN4148 只有150mA, 建议加大。