This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

UCD9090: UCD9090-Q1

Part Number: UCD9090

我们的一个项目中使用了TI的电源时序控制芯片UCD9090-Q1,使用Fusion GUI进行程序烧写后,重新上电程序失效。

具体情况如下:调试完毕,点击了“write to hardware”和“store RAM to Flash”后,与PC连接过程中(通过USB转GPIO工具)对产品上电,能在PC端监控到电源正常,但是脱离PC重新上电之后,除了初始电源,后续电源都是0V,怀疑程序并没有写入Flash,掉电后程序从RAM中丢失。

想问一下:1、有没有什么办法可以检测程序是否写入FLASH;

2、使用Fusion GUI的流程细则,操作指南中的work flow 在 save to file 这一步是怎么操作的?如何保证操作之后程序写入FLASH?

求大神帮忙解决一下,谢谢!