This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

TPS56221: 有的板子初次上电TPS56221的输入和输就短路烧坏

Part Number: TPS56221

我板上用12v供电,TPS56221产生1.5V,多数板子能正常上电,有的板子初次上电就TPS56221的输入和输出TPS56221_1V5.pdf就短路,请问是电路哪里不对吗?

  • HI

        绝大部分板子正常工作电路应该问题不大,你可以按照datasheet上的案例来确认一下(Page16),  主要就是补偿电路麻烦点。

        但是补偿电路略微偏差一般不会造成芯片内部MOS烧掉,你需要确认功率电感电感饱和电流足够,其次输入没有热插拔或者硬开关之类(需要是软开关控制,电压输入时不会产生较大的电压震荡)

  • 功率电感电感饱和电流39A应该够了,EN/SS的管脚上没有焊软启动电容,是由FPGA控制MOS管(BSS138),使其上电为低电平延时后再变为高阻,使TPS56221上电,这算是硬开关还是软开关?这样会产生电压较大震荡吗?有些板子是在烧写完FPGA程序之后TPS56221就烧坏

  • Hi

        直接测试启动瞬间的输入电压(用示波器)来确认。