Hi TI team,
LM5140-Q1 DS里有这么一句话:
The MOSFETs used with the LM5140 require a logic-level gate threshold with on-resistance
specified with VGS = 4.5 V or lower。
但是目前由于市场上logic level的MOS管比较难购买,是否能使用standard level的MOS管,如BUK7K6R2?如果不能具体是什么原因
This thread has been locked.
If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.
Hi TI team,
LM5140-Q1 DS里有这么一句话:
The MOSFETs used with the LM5140 require a logic-level gate threshold with on-resistance
specified with VGS = 4.5 V or lower。
但是目前由于市场上logic level的MOS管比较难购买,是否能使用standard level的MOS管,如BUK7K6R2?如果不能具体是什么原因
HI
这个芯片驱动供电Vcc是5V(最小4.75V), 相比其他芯片很多都是VCC 6V, 甚至7V以上,要低一些。所以可能是因为这个要求选择的MOS Vth偏低一点。
低温下,最低4.5V, 如果你应用环境温度会相对比较低, 不建议选择这个。 Vth 2~3V的MOS 很多,最多放低到3.5V.
最好的情况如上,直接用样片来测试看看,确认一下波形。