This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

LM5140-Q1: MOS管选型

Part Number: LM5140-Q1


Hi TI team,

      LM5140-Q1 DS里有这么一句话:

The MOSFETs used with the LM5140 require a logic-level gate threshold with on-resistance
specified with VGS = 4.5 V or lower。

但是目前由于市场上logic level的MOS管比较难购买,是否能使用standard level的MOS管,如BUK7K6R2?如果不能具体是什么原因