Part Number: TPS63050
TPS63050
输入3.1-3.5V,输出2.5V
使用电子负载。
当负载电流为0.7A时,输出电压为2.53V
当负载电流为0.8A时,芯片会down,输出会降低到0V左右。
根据datasheet,降压模式时,持续输出电流会达到1A,为什么在0.8A的时候就不能用了?
This thread has been locked.
If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.
Part Number: TPS63050
TPS63050
输入3.1-3.5V,输出2.5V
使用电子负载。
当负载电流为0.7A时,输出电压为2.53V
当负载电流为0.8A时,芯片会down,输出会降低到0V左右。
根据datasheet,降压模式时,持续输出电流会达到1A,为什么在0.8A的时候就不能用了?
HI
电流限制(保护)了,这个芯片虽然说如果降压下,最大输出典型值是1A, 但是并非最小电流,选择芯片是需要按照最小(最恶劣情况)来设计。
而用webench设计,这个芯片在上述条件上最大输出略多于最大输出0.6A。