This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

TPS63050: 降压模式,期望输出2.5V/0.8A时,芯片不work

Part Number: TPS63050


TPS63050

输入3.1-3.5V,输出2.5V

使用电子负载。

当负载电流为0.7A时,输出电压为2.53V

当负载电流为0.8A时,芯片会down,输出会降低到0V左右。

根据datasheet,降压模式时,持续输出电流会达到1A,为什么在0.8A的时候就不能用了?

  • HI

       电流限制(保护)了,这个芯片虽然说如果降压下,最大输出典型值是1A, 但是并非最小电流,选择芯片是需要按照最小(最恶劣情况)来设计。

       而用webench设计,这个芯片在上述条件上最大输出略多于最大输出0.6A。