This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

LM5022: 过流保护

Part Number: LM5022

在调试LM5022芯片时,遇到如下问题,请帮忙解答。

1、关于限流电阻值的计算,datasheet中给的公式如下红框处,请帮忙解释一下为什么要考虑VCL/ILIM以外的项,式中(Vo-Vin)*3*D/( L*Fsw)表示什么意思?

2、RS2除了对限流有影响外,还有其它什么作用,阻值能否取0?也就是说限流靠内部2KΩ、RS1、RSNS来决定。

当前我们将RS2取0的时候,芯片工作会异常,如下图“原边电感电流波形”所示,在电流没有达到限流的情况下,一个周期占空比很高,一个周期占空比很低,很不稳定。

3、调试中为了debug问题,我们有尝试过将下图中R198 NC,C194替换为0R,发现很快触发过流保护;此时CS引脚2K电阻到GND,根据LM5022内部框图,是不会触发内部过流保护的。请帮忙分析原因。

  • HI

        1.  datasheet没有提供推到的过程,从datasheet看描述不是特别清楚,按照描述推到有些困难。

        2. Rs2不能取值0ohm。

        3. 会影响的,特别是C194影响很大。

  • 追问一下:

    1.Rs2不能取0ohm的原因;

    2.C194作用是什么,为何一定要要在CS引脚加一个电容,最重要的是,请帮忙确认一下C194电容的值应该如何选取。

  • HI

         见datasheet描述:

         This current flows through an internal 2-kΩ resistor to create a minimum compensation ramp with a slope of 100 mV × ƒSW (typical). The slope of the compensation ramp increases when external resistance is added for filtering the current sense (RS1) or in the position RS2. As shown in Figure 12 and the Functional Block Diagram, the sensed current slope and the compensation slope add together to create the signal used for current limiting and for the control loop itself.