我们的项目中要求使用PWRON上接个按钮来控制上电,所以将PWRHOLD接个上拉电阻到vaux3,现在能通过PWRON上的按钮来控制开关机了,但我们还想通过设置PMIC上的RTC alarm来定时开机,这样该如何处理呢,是不是电路只要将INT1接个电阻到VBTA就可以了?然后软件中设置65910中的ALARM相关寄存器设置时间,和使能RTC_INTERRUPTS_REG.IT_ALARM就行了?
This thread has been locked.
If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.
我们的项目中要求使用PWRON上接个按钮来控制上电,所以将PWRHOLD接个上拉电阻到vaux3,现在能通过PWRON上的按钮来控制开关机了,但我们还想通过设置PMIC上的RTC alarm来定时开机,这样该如何处理呢,是不是电路只要将INT1接个电阻到VBTA就可以了?然后软件中设置65910中的ALARM相关寄存器设置时间,和使能RTC_INTERRUPTS_REG.IT_ALARM就行了?
我的PWRON上的上拉电阻本来就是接到VBAT上的,我在内核里强制设置了RTC-ALARM的告警时间,并且把INT_STS_REG和INT_STS_REG2都清0了,再将RTC_INTERRUPTS_REG中的IT_ALARM设置为1,然后关机(tps65910在POWER OFF状态,只有RTC在工作),可到时间后,并没有启动啊!
我将INT1接上拉10K到vbat,关机量出的电平却只有0.8v左右,这又是怎么回事?