This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

关于tps65910的软开机功能

Other Parts Discussed in Thread: TPS65910

我们的项目中要求使用PWRON上接个按钮来控制上电,所以将PWRHOLD接个上拉电阻到vaux3,现在能通过PWRON上的按钮来控制开关机了,但我们还想通过设置PMIC上的RTC alarm来定时开机,这样该如何处理呢,是不是电路只要将INT1接个电阻到VBTA就可以了?然后软件中设置65910中的ALARM相关寄存器设置时间,和使能RTC_INTERRUPTS_REG.IT_ALARM就行了?

  • Hi,

    可以这样实现,但须注意下述说明:

    触发POWER-ON使能条件仅在中断状态位初始时为低,中断状态寄存器中无之前相同的待处理中断。

    另外PWRON上的上拉电阻也建议接到VBAT上。

    Thanks.

  • 我的PWRON上的上拉电阻本来就是接到VBAT上的,我在内核里强制设置了RTC-ALARM的告警时间,并且把INT_STS_REG和INT_STS_REG2都清0了,再将RTC_INTERRUPTS_REG中的IT_ALARM设置为1,然后关机(tps65910在POWER OFF状态,只有RTC在工作),可到时间后,并没有启动啊!

    我将INT1接上拉10K到vbat,关机量出的电平却只有0.8v左右,这又是怎么回事?