This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

LM51581: LM51581RTER输出电流能力确认

Part Number: LM51581

LM51581输出电流能力,datasheet描述是1.63~2.12A,但是当我在WEBENCH POWER DESIGNER模拟计算的时候,工具里的范围只能是0.5A以内,计算条件:VIN=24V,VOUT=53V/0.6A,fre=0.65Mhz,请帮忙确认下LM51581RTER的真实输出电流能力,谢谢!

  • Hi

         你提到的1.63~2.12是开关的限制电流,需要按照最恶劣情况设计,所以电流保护点为1.63A, 也就是最大输入峰值电流。

         以升压电路而言,输入峰值电流是最大输入电流的1.15倍(即电感的纹波电流为输入电流的0.3倍)

         所以最大输入功率为1.63/1.15* 24V  (即最大输入电流乘以输入电压),  假设电源转换效率为85%

         那么最大输出功率就是1.63/1.15* 24* 0.85

         最大输出功率除以输出电压就可以估算出最大输出电流。

         以上即估算最大输出电流的方法。