This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

BQ2970: BQ29700DSER-Protection

Part Number: BQ2970


Customer use BQ29700DSER protection IC  which is used on PCB Control board and separated from the battery.

The application requires that the battery protection IC can meet the function of protecting the battery. At the same time, replacing the battery does not require additional operation of the battery to power the device.(Now when replace the battery,they must to charge the battery,the control board can work.)

So do we have this device like customer needed?