Customer use BQ29700DSER protection IC which is used on PCB Control board and separated from the battery.
The application requires that the battery protection IC can meet the function of protecting the battery. At the same time, replacing the battery does not require additional operation of the battery to power the device.(Now when replace the battery,they must to charge the battery,the control board can work.)
So do we have this device like customer needed?