This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

各位专家,我想问一下关于PL900之VOUT输出Vbat或Vpack时的疑问?



在手册中:

当VOUT设置为测量Vbat时,进行下面设置:

The total pack voltage can also be monitored. The BAT voltage output is enabled or disabled by
FUNCTION_CONTROL [BAT].

VOUT4 = (Total battery voltage) × 0.02 when BAT = 1

当设置VOUT为Vpack时,进行下面设置:

The total pack voltage can also be monitored. The PACK voltage output is enabled or disabled by
FUNCTION_CONTROL [PACK].
VOUT3 = (Total pack voltage) × 0.02 when PACK = 1

但是在实际测量时,不管修改输出为VPACK或是VBAT输出的值总是不对,输出的值按照公式计算后,约为实际值的一半左右。

当使用ev300控制时,输出的电压也是不对的,不知道为什么,

希望能得到专家的解答。

我的qq:15738395