This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

LP8556: 在设计恒流源芯片LP8556的时候,出现了恒流无法控制的问题

Part Number: LP8556

使用LP8556SQE-E08/NOPB 来控制LED背光,4路,单路6ma电流,16.5V电压,原理图如下:

软件设置方法如下:

首先0x16设置为0x00,设置1-4路LED不使能,然后0xa2设置为0x00,比例算法设为方式0,0xa0设置为0x99,比例为6/10,最大电流设为10ma,比例为6/10,最后0x16设置为0x0f,设置1-4路LED使能

输入电压是12V,I2C 寄存器可以正常设置,出现无法控制恒流问题,LED无法点亮,VOOST电压在14V

通过将灯的LED-直接接到地,手动将lp8556的BOOST控制到17V,屏幕有可以点亮,

电路连接没有问题,帮忙看看有什么问题

中间串了测电流的芯片,去电也没影响。

谢谢

  • Hi

       没有太明白你的意思,建议你先不配置寄存器(采用默认配置), 做出4路10mA输出,LED电压是VF决定,参考datasheet电路,主要设置一下电流,和频率。

       正常之后,再通过调光设置输出6mA.