This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

BQ24081: BQ24081 charge issue

Part Number: BQ24081


目前使用BQ24081充一個250mAh的電池,設計使用200mA充電,經實測,大約1.5小時後,

電池電壓已經到4.18V,充電電流開始下降,幾乎已經不再充電,代表此時電池已充飽電,但

是STAT1 pin,還是輸出為0V,沒有任何變化,也就是BQ24081並沒有透過該pin告知已充飽

電.

我試著外加一個4.25V的電壓給電池,此時STAT1 pin產生變化,輸出3.3V,代表STAT1 pin是

有動作的,只是當時電池沒有達到要求的電壓,所以STAT1 pin沒有動作,但電池只要充到4.18V

便會停止充電.,所以沒辦法達到STAT1 pin要求動作的電壓.

我另外使用一個規格4.4V的電池進行充電,也是達到4.18V便停止充電,代表不是電池的問題,

請問是否有人可以協助解決該問題.

  • 您好,数据手册的电器性能表中介绍Vout4.2V, 在25度时有+-0.35%的误差,4.18V应该也是可以的。

    建议检查II(TERM)的设置,请参考7.3.5 Charge Termination Detection and Recharge

  • 參考7.3.5文件,Charge截止電流經計算為20mA,但實際測試,Charge充電電流大約要低於5mA以下才會截止,麻煩確認,謝謝.

  • 您好,请确认截止电压是否满足条件。

  • 經測試,當充電電流降到20mA時,此時截止電壓大約是250mV,但此時STAT1 pin還是沒有變化,持續量測,當充電電流降到13mA時,截止電壓大約是158mV,當充電電流降到8mA時,截止電壓大約是95mV,當充電電流降到4mA時,截止電壓大約是40mV,此時STAT1還是都沒變化,一直到充電電流降到大約2mA時,STAT1 pin才有變化,此時才截止充電.

  • 您好,除电池外输出端是否连接了其它电路?您在哪里测量电池电流?您是用数字式万用表测量还是gauge读到的?

    如果有任何连接在输出引脚(与电池并联)上的电池,请将其移除。

  • 我們大部分時間都是量測IN端的輸入電流,我們也有試著直接量測電池端的電流,大約差1mA,差異不大,IN端我們使用USB電流表量測,電池端我們使用數字式萬用表量測,電池端我們連接我們的負載,在量測期間,為了避免干擾,負載端都是不開機的,也就是負載端不耗電.

  • 您好,The only reason it would not terminate is if the output voltage were not at the regulation voltage or if the voltage on ISET were not below 0.25V for a time longer than the deglitch period of 375 ms.  Thus, I would also suggest that you look at the output voltage and ISET pins with a scope and a timescale of around 100 ms to see if anything is disturbing those voltages to cause the deglitch timer to reset.

  • 經測試,發現跟輸入5V電源有關,不確定是否因為輸入5V電源的不穩定,造成ISET截止電壓有問題,我們實測5V電源,上面會有一個凸波雜訊,

    我們使用不同的變壓器,量測5V雜訊的peak-to-peak,當pk-pk=522mV時,截止電流為1mA,當pk-pk=288mV時,截止電流為13mA,當pk-pk=232mV時,截止電流為18mA,

  • 您好,建议您换一个电源验证一下是不是电源的问题造成的。