This thread has been locked.
If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.
我们客户需要设计12V->24V 峰值输出60A,稳定工作在40A的DCDC产品,目前选型用LM5122来进行多相驱动。
不知道该用几相合适呢?工作频率设置在多少比较合适呢?
比如100KHz 与 250KHz,这二者在稳定性上会有太大的差异吗?求教了~谢谢~
Hi
可以采用两片芯片并联, 工作频率不建议设计太高,建议200~300kHz是可以的,要特别注意MOS的选择,因为如果是2相设计输入电流单路都超过50A.
所以选择3片并联更好。
比如,我们选用4相位并联,是不是就是按照2相设计一样,继续如法炮制,级联4路芯片就可以了呢?
那么,输入与输出电容呢?是不是也是按照单相指标来设计,然后直接并联即可呢?
HI
有些差异,如果是四片芯片并联,你可以看看datasheet上级联的参考电路,需要四路90°相差的同步信号输入,或者2个两相并联。