This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

LM5122: 使用LM5122设计12V->24V 峰值输出60A,稳定工作在40A的DCDC产品,该用几相并联呢?

Part Number: LM5122

我们客户需要设计12V->24V 峰值输出60A,稳定工作在40A的DCDC产品,目前选型用LM5122来进行多相驱动。

不知道该用几相合适呢?工作频率设置在多少比较合适呢?

比如100KHz 与 250KHz,这二者在稳定性上会有太大的差异吗?求教了~谢谢~

x 出现错误。请重试或与管理员联系。