Other Parts Discussed in Thread: CSD18540Q5B
如下图,使用LM25116和CSD18540Q5B将24V降压到5V,在空载时,24V电源显示为0.06A,PQ1温度50度左右,PQ2温度45度左右;在5V抽载5A时,PQ1温度85度左右,PQ2温度80度左右,在5V抽载13A时,温度会短时间内上升到120多度,这三个情况都不符合理论设计,如果将输入电源从24V降到12V,温度上升明显要慢,温度要低一点。SW引脚波形如下图。电感的内阻2.2mohm,饱和电流23A,感值也较合理;MOS管的RDS(ON)也是只有1.8mohm,理论上符合设计,是什么原因导致MOS发热严重