This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

BQ34110: 條件沒到就100%了

Part Number: BQ34110

你好,

请帮忙看一下这个log 跟设定

使用bq34110 铁锂电芯 11串1并 60Ah

因为电芯容量太大所以写为 6Ah. 有将电流相关的参数都改为1/10

发现满充条件还没满足的状况下 FC=1直接变100%了

请帮忙看一下设定是否错误

谢谢!20220906.gg.csv

Wed Sep 07 11:00:39 CST 2022

Device Version Info = 0110_0_02
BQZ Device Name = bq34110
BQZ Firmware Version = 0_02

Design Capacity = 6000

Sample,DateTime,ElapsedTime,Control,Temperature,Voltage,Batt Stat,Current,RemCap,FullChgCap,AvgCurr,RunTimeEmty,AvgTimeFull,AccumulatedCharge,AccumulatedCharge Time,AvgPwr,IntTemp,CycleCnt,RSOC,SOH,ChgVolt,ChgCurr,OpStat,GaugeStat,CEDVRemCap,EDV Threshold,SmRemCap,SmCurrent,ManufacStat,EOSLearnStatus,EOSSafetyStatus,EOSStatus,AutoLearnTime,AvgDsgCurrent,AvgDsgTemp,LearnedResistance,LearnedResTimeHours,LearnedResTimeSeconds,LastLearnedResistance,LastLearnedResHours,LastLearnedResSeconds,InitialRRateAgeHours,InitialRRateAgeSeconds,RRate,RRateLong,InitialRcellRRateLearnRes,InitialRcellRRateLearnCount,LogRowTime(ms),LogStatus
1,2022-09-07 11:00:44,5.013,0x0000,25.5,34001,0x0098,0,5603,5603,0,65535,65535,0,0,0,25.2,2,100,93,38500,0,0x0282,0x54A,5603,3000,5603,0,0x00,0x0000,0x00,0x00,0,0,-273.2,0,0,0,0,0,0,0,0,0,0,0,0,560,SUCCESS
2,2022-09-07 11:00:49,10.015,0x0000,25.5,34001,0x0098,0,5603,5603,0,65535,65535,0,0,0,25.2,2,100,93,38500,0,0x0282,0x54A,5603,3000,5603,0,0x00,0x0000,0x00,0x00,0,0,-273.2,0,0,0,0,0,0,0,0,0,0,0,0,560,SUCCESS
3,2022-09-07 11:00:54,15.381,0x0000,25.5,34001,0x0098,0,5603,5603,0,65535,65535,0,0,0,25.2,2,100,93,38500,0,0x0282,0x54A,5603,3000,5603,0,0x00,0x0000,0x00,0x00,0,0,-273.2,0,0,0,0,0,0,0,0,0,0,0,0,570,SUCCESS
4,2022-09-07 11:00:59,20.025,0x0000,25.5,34001,0x0098,0,5603,5603,0,65535,65535,0,0,0,25.2,2,100,93,38500,0,0x0282,0x54A,5603,3000,5603,0,0x00,0x0000,0x00,0x00,0,0,-273.2,0,0,0,0,0,0,0,0,0,0,0,0,566,SUCCESS
5,2022-09-07 11:01:04,25.027,0x0000,25.6,32560,0x4005,-3043,160,5347,-885,11,65535,0,0,-262,25.3,2,3,89,38500,6000,0x028A,0x6044,160,3069,160,0,0x00,0x0000,0x00,0x00,0,0,-273.2,0,0,0,0,0,0,0,0,0,0,0,0,563,SUCCESS
6,2022-09-07 11:01:09,30.042,0x0000,25.6,32450,0x4025,-3043,0,5347,-1512,0,65535,0,0,-447,25.3,2,0,89,38500,6000,0x028A,0x6065,0,3000,0,0,0x00,0x0000,0x00,0x00,0,0,-273.2,0,0,0,0,0,0,0,0,0,0,0,0,565,SUCCESS
7,2022-09-07 11:01:14,35.414,0x0000,25.6,32846,0x4025,0,0,5347,-1647,0,65535,0,0,-486,25.3,2,0,89,38500,6000,0x028A,0x6065,0,3000,0,0,0x00,0x0000,0x00,0x00,0,0,-273.2,0,0,0,0,0,0,0,0,0,0,0,0,566,SUCCESS
8,2022-09-07 11:01:19,40.060,0x0000,25.6,32912,0x40A5,0,0,5347,-1168,0,65535,0,0,-345,25.3,2,0,89,38500,6000,0x028A,0x6065,0,3000,0,0,0x00,0x0000,0x00,0x00,0,0,-273.2,0,0,0,0,0,0,0,0,0,0,0,0,562,SUCCESS
9,2022-09-07 11:01:24,45.066,0x0000,25.6,32912,0x40A5,0,0,5347,-828,0,65535,0,0,-245,25.3,2,0,89,38500,6000,0x028A,0x6065,0,3000,0,0,0x00,0x0000,0x00,0x00,0,0,-273.2,0,0,0,0,0,0,0,0,0,0,0,0,571,SUCCESS
10,2022-09-07 11:01:29,50.069,0x0000,25.6,32912,0x40A5,0,0,5347,-588,0,65535,0,0,-174,25.3,2,0,89,38500,6000,0x028A,0x6065,0,3000,0,0,0x00,0x0000,0x00,0x00,0,0,-273.2,0,0,0,0,0,0,0,0,0,0,0,0,569,SUCCESS
11,2022-09-07 11:01:34,55.075,0x0000,25.6,32912,0x40A5,0,0,5347,-417,0,65535,0,0,-123,25.2,2,0,89,38500,6000,0x028A,0x6065,0,3000,0,0,0x00,0x0000,0x00,0x00,0,0,-273.2,0,0,0,0,0,0,0,0,0,0,0,0,561,SUCCESS
12,2022-09-07 11:01:39,60.081,0x0000,25.6,33198,0x40A5,0,0,5347,-296,0,65535,0,0,-87,25.2,2,0,89,38500,6000,0x028A,0x6065,0,3000,0,0,0x00,0x0000,0x00,0x00,0,0,-273.2,0,0,0,0,0,0,0,0,0,0,0,0,572,SUCCESS
13,2022-09-07 11:01:44,65.093,0x0000,25.6,33198,0x40A5,0,0,5347,-210,0,65535,0,0,-62,25.2,2,0,89,38500,6000,0x028A,0x6065,0,3000,0,0,0x00,0x0000,0x00,0x00,0,0,-273.2,0,0,0,0,0,0,0,0,0,0,0,0,561,SUCCESS
14,2022-09-07 11:01:49,70.097,0x0000,25.6,33198,0x40A5,0,0,5347,-149,0,65535,0,0,-44,25.2,2,0,89,38500,6000,0x028A,0x6065,0,3000,0,0,0x00,0x0000,0x00,0x00,0,0,-273.2,0,0,0,0,0,0,0,0,0,0,0,0,573,SUCCESS
15,2022-09-07 11:01:54,75.104,0x0000,25.6,33198,0x40A5,0,0,5347,-105,0,65535,0,0,-31,25.3,2,0,89,38500,6000,0x028A,0x6065,0,3000,0,0,0x00,0x0000,0x00,0x00,0,0,-273.2,0,0,0,0,0,0,0,0,0,0,0,0,563,SUCCESS
16,2022-09-07 11:01:59,80.111,0x0000,25.6,33286,0x40A5,0,0,5347,-75,0,65535,0,0,-22,25.3,2,0,89,38500,6000,0x028A,0x6065,0,3000,0,0,0x00,0x0000,0x00,0x00,0,0,-273.2,0,0,0,0,0,0,0,0,0,0,0,0,589,SUCCESS
17,2022-09-07 11:02:04,85.115,0x0000,25.6,33286,0x40A5,0,0,5347,-53,0,65535,0,0,-16,25.3,2,0,89,38500,6000,0x028A,0x6065,0,3000,0,0,0x00,0x0000,0x00,0x00,0,0,-273.2,0,0,0,0,0,0,0,0,0,0,0,0,568,SUCCESS
18,2022-09-07 11:02:09,90.121,0x0000,25.6,33286,0x40A5,0,0,5347,-38,0,65535,0,0,-11,25.3,2,0,89,38500,6000,0x028A,0x6065,0,3000,0,0,0x00,0x0000,0x00,0x00,0,0,-273.2,0,0,0,0,0,0,0,0,0,0,0,0,564,SUCCESS
19,2022-09-07 11:02:14,95.124,0x0000,25.6,33286,0x40A4,0,0,5347,-27,0,65535,0,0,-8,25.2,2,0,89,38500,6000,0x0282,0x45,0,3000,0,0,0x00,0x0000,0x00,0x00,0,0,-273.2,0,0,0,0,0,0,0,0,0,0,0,0,560,SUCCESS
20,2022-09-07 11:02:19,100.126,0x0000,25.6,33330,0x40A4,0,0,5347,-19,0,65535,0,0,-6,25.2,2,0,89,38500,6000,0x0282,0x45,0,3000,0,0,0x00,0x0000,0x00,0x00,0,0,-273.2,0,0,0,0,0,0,0,0,0,0,0,0,573,SUCCESS
21,2022-09-07 11:02:24,105.131,0x0000,25.6,33330,0x40A4,0,0,5347,-13,0,65535,0,0,-4,25.2,2,0,89,38500,6000,0x0282,0x45,0,3000,0,0,0x00,0x0000,0x00,0x00,0,0,-273.2,0,0,0,0,0,0,0,0,0,0,0,0,570,SUCCESS
22,2022-09-07 11:02:29,110.134,0x0000,25.6,33330,0x40A4,0,0,5347,-10,0,65535,0,0,-3,25.2,2,0,89,38500,6000,0x0282,0x45,0,3000,0,0,0x00,0x0000,0x00,0x00,0,0,-273.2,0,0,0,0,0,0,0,0,0,0,0,0,566,SUCCESS
23,2022-09-07 11:02:34,115.142,0x0000,25.6,33330,0x40A4,0,0,5347,-7,0,65535,0,0,-2,25.1,2,0,89,38500,6000,0x0282,0x45,0,3000,0,0,0x00,0x0000,0x00,0x00,0,0,-273.2,0,0,0,0,0,0,0,0,0,0,0,0,574,SUCCESS
24,2022-09-07 11:02:39,120.155,0x0000,25.6,33363,0x40A4,0,0,5347,-5,0,65535,0,0,-1,25.1,2,0,89,38500,6000,0x0282,0x45,0,3000,0,0,0x00,0x0000,0x00,0x00,0,0,-273.2,0,0,0,0,0,0,0,0,0,0,0,0,558,SUCCESS
25,2022-09-07 11:02:44,125.160,0x0000,25.6,33363,0x40A4,0,0,5347,-3,0,65535,0,0,-1,25.1,2,0,89,38500,6000,0x0282,0x45,0,3000,0,0,0x00,0x0000,0x00,0x00,0,0,-273.2,0,0,0,0,0,0,0,0,0,0,0,0,571,SUCCESS
26,2022-09-07 11:02:49,130.169,0x0000,25.6,33363,0x40A4,0,0,5347,-2,0,65535,0,0,-1,25.1,2,0,89,38500,6000,0x0282,0x45,0,3000,0,0,0x00,0x0000,0x00,0x00,0,0,-273.2,0,0,0,0,0,0,0,0,0,0,0,0,561,SUCCESS
27,2022-09-07 11:02:54,135.178,0x0000,25.6,33363,0x40A4,0,0,5347,-2,0,65535,0,0,-1,25.1,2,0,89,38500,6000,0x0282,0x45,0,3000,0,0,0x00,0x0000,0x00,0x00,0,0,-273.2,0,0,0,0,0,0,0,0,0,0,0,0,599,SUCCESS
28,2022-09-07 11:02:59,140.186,0x0000,25.6,33396,0x40A4,0,0,5347,-1,0,65535,0,0,0,25.1,2,0,89,38500,6000,0x0282,0x45,0,3000,0,0,0x00,0x0000,0x00,0x00,0,0,-273.2,0,0,0,0,0,0,0,0,0,0,0,0,561,SUCCESS
29,2022-09-07 11:03:04,145.193,0x0000,25.6,33396,0x40A4,0,0,5347,-1,0,65535,0,0,0,25.1,2,0,89,38500,6000,0x0282,0x45,0,3000,0,0,0x00,0x0000,0x00,0x00,0,0,-273.2,0,0,0,0,0,0,0,0,0,0,0,0,569,SUCCESS
30,2022-09-07 11:03:09,150.198,0x0000,25.6,33396,0x40A4,0,0,5347,-1,0,65535,0,0,0,25.1,2,0,89,38500,6000,0x0282,0x45,0,3000,0,0,0x00,0x0000,0x00,0x00,0,0,-273.2,0,0,0,0,0,0,0,0,0,0,-256,-1,564,SUCCESS
31,2022-09-07 11:03:14,155.213,0x0000,25.6,33396,0x40A4,0,0,5347,0,65535,65535,0,0,0,25.0,2,0,89,38500,6000,0x0282,0x45,0,3000,0,0,0x00,0x0000,0x00,0x00,0,0,-273.2,0,0,0,0,0,0,0,0,0,0,0,0,563,SUCCESS
32,2022-09-07 11:03:19,160.214,0x0000,25.6,33407,0x40A4,0,0,5347,0,65535,65535,0,0,0,25.0,2,0,89,38500,6000,0x0282,0x45,0,3000,0,0,0x00,0x0000,0x00,0x00,0,0,-273.2,0,0,0,0,0,0,0,0,0,0,0,0,580,SUCCESS
33,2022-09-07 11:03:24,165.218,0x0000,25.6,33407,0x40A4,0,0,5347,0,65535,65535,0,0,0,25.0,2,0,89,38500,6000,0x0282,0x45,0,3000,0,0,0x00,0x0000,0x00,0x00,0,0,-273.2,0,0,0,0,0,0,0,0,0,0,0,0,574,SUCCESS
34,2022-09-07 11:03:29,170.228,0x0000,25.6,33407,0x40A4,0,0,5347,0,65535,65535,0,0,0,25.0,2,0,89,38500,6000,0x0282,0x45,0,3000,0,0,0x00,0x0000,0x00,0x00,0,0,-273.2,0,0,0,0,0,0,0,0,0,0,0,0,563,SUCCESS
35,2022-09-07 11:03:34,175.237,0x0000,25.6,33407,0x40A4,0,0,5347,0,65535,65535,0,0,0,25.0,2,0,89,38500,6000,0x0282,0x05,0,3000,0,0,0x00,0x0000,0x00,0x00,0,0,-273.2,0,0,0,0,0,0,0,0,0,0,0,0,585,SUCCESS
36,2022-09-07 11:03:39,180.249,0x0000,25.6,33836,0x4026,900,1,5347,261,65535,1229,0,0,80,25.1,2,1,89,38500,6000,0x0282,0x05,1,3000,1,0,0x00,0x0000,0x00,0x00,0,0,-273.2,0,0,0,0,0,0,0,0,0,0,0,0,559,SUCCESS
37,2022-09-07 11:03:44,185.252,0x0000,25.6,33880,0x4026,898,2,5347,447,65535,717,0,0,137,25.2,2,1,89,38500,6000,0x0282,0x05,2,3000,2,0,0x00,0x0000,0x00,0x00,0,0,-273.2,0,0,0,0,0,0,0,0,0,0,0,0,571,SUCCESS
38,2022-09-07 11:03:49,190.260,0x0000,25.6,33935,0x4026,898,3,5347,578,65535,555,0,0,178,25.2,2,1,89,38500,6000,0x0282,0x05,4,3000,4,0,0x00,0x0000,0x00,0x00,0,0,-273.2,0,0,0,0,0,0,0,0,0,0,0,0,564,SUCCESS
39,2022-09-07 11:03:54,195.261,0x0000,25.6,33979,0x4026,898,5,5347,671,65535,478,0,0,207,25.2,2,1,89,38500,6000,0x0282,0x05,5,3000,5,0,0x00,0x0000,0x00,0x00,0,0,-273.2,0,0,0,0,0,0,0,0,0,0,0,0,563,SUCCESS
40,2022-09-07 11:03:59,200.266,0x0000,25.6,34012,0x4026,900,6,5347,737,65535,435,0,0,227,25.2,2,1,89,38500,6000,0x0282,0x05,6,3000,6,0,0x00,0x0000,0x00,0x00,0,0,-273.2,0,0,0,0,0,0,0,0,0,0,0,0,565,SUCCESS
41,2022-09-07 11:04:04,205.266,0x0000,25.6,34056,0x4026,900,7,5347,784,65535,409,0,0,242,25.2,2,1,89,38500,6000,0x0282,0x05,7,3000,7,0,0x00,0x0000,0x00,0x00,0,0,-273.2,0,0,0,0,0,0,0,0,0,0,0,0,573,SUCCESS
42,2022-09-07 11:04:09,210.269,0x0000,25.6,34089,0x4026,898,8,5347,818,65535,392,0,0,253,25.2,2,1,89,38500,6000,0x0282,0x05,9,3000,9,0,0x00,0x0000,0x00,0x00,0,0,-273.2,0,0,0,0,0,0,0,0,0,0,0,0,586,SUCCESS
43,2022-09-07 11:04:14,215.276,0x0000,25.6,34133,0x4026,900,10,5347,841,65535,381,0,0,260,25.2,2,1,89,38500,6000,0x0282,0x05,10,3000,10,0,0x00,0x0000,0x00,0x00,0,0,-273.2,0,0,0,0,0,0,0,0,0,0,0,0,564,SUCCESS
44,2022-09-07 11:04:19,220.280,0x0000,25.6,34166,0x4026,900,11,5347,858,65535,373,0,0,266,25.2,2,1,89,38500,6000,0x0282,0x05,11,3000,11,0,0x00,0x0000,0x00,0x00,0,0,-273.2,0,0,0,0,0,0,0,0,0,0,0,0,560,SUCCESS
45,2022-09-07 11:04:24,225.285,0x0000,25.6,34199,0x4026,898,12,5347,870,65535,368,0,0,270,25.2,2,1,89,38500,6000,0x0282,0x05,12,3000,12,0,0x00,0x0000,0x00,0x00,0,0,-273.2,0,0,0,0,0,0,0,0,0,0,0,0,570,SUCCESS
46,2022-09-07 11:04:29,230.286,0x0000,25.6,34221,0x4026,898,13,5347,878,65535,365,0,0,272,25.2,2,1,89,38500,6000,0x0282,0x05,13,3000,14,0,0x00,0x0000,0x00,0x00,0,0,-273.2,0,0,0,0,0,0,0,0,0,0,0,0,570,SUCCESS
47,2022-09-07 11:04:34,235.289,0x0000,25.6,34254,0x4026,898,15,5347,884,65535,362,0,0,274,25.2,2,1,89,38500,6000,0x0282,0x05,15,3000,15,0,0x00,0x0000,0x00,0x00,0,0,-273.2,0,0,0,0,0,0,0,0,0,0,0,0,565,SUCCESS
48,2022-09-07 11:04:39,240.304,0x0000,25.6,34287,0x4026,900,16,5347,888,65535,360,0,0,276,25.3,2,1,89,38500,6000,0x0282,0x05,16,3000,16,0,0x00,0x0000,0x00,0x00,0,0,-273.2,0,0,0,0,0,0,0,0,0,0,0,0,584,SUCCESS
49,2022-09-07 11:04:44,245.311,0x0000,25.6,34320,0x4026,900,17,5347,891,65535,359,0,0,277,25.3,2,1,89,38500,6000,0x0282,0x05,17,3000,17,0,0x00,0x0000,0x00,0x00,0,0,-273.2,0,0,0,0,0,0,0,0,0,0,0,0,560,SUCCESS
50,2022-09-07 11:04:49,250.321,0x0000,25.6,34342,0x4026,898,18,5347,893,65535,358,0,0,278,25.3,2,1,89,38500,6000,0x0282,0x05,18,3000,18,0,0x00,0x0000,0x00,0x00,0,0,-273.2,0,0,0,0,0,0,0,0,0,0,0,0,567,SUCCESS
51,2022-09-07 11:04:54,255.323,0x0000,25.6,34364,0x401A,900,5347,5347,895,65535,0,0,0,279,25.3,2,100,89,38500,6000,0x0282,0x0A,5347,3000,5347,0,0x00,0x0000,0x00,0x00,0,0,-273.2,0,0,0,0,0,0,0,0,0,0,0,0,563,SUCCESS
52,2022-09-07 11:04:59,260.330,0x0000,25.6,34397,0x001A,898,5347,5347,896,65535,0,0,0,279,25.3,2,100,89,38500,0,0x0282,0x0A,5347,3000,5347,0,0x00,0x0000,0x00,0x00,0,0,-273.2,0,0,0,0,0,0,0,0,0,0,0,0,573,SUCCESS
53,2022-09-07 11:05:04,265.335,0x0000,25.6,34419,0x001A,898,5347,5347,896,65535,0,0,0,280,25.3,2,100,89,38500,0,0x0282,0x0A,5347,3000,5347,0,0x00,0x0000,0x00,0x00,0,0,-273.2,0,0,0,0,0,0,0,0,0,0,0,0,583,SUCCESS
54,2022-09-07 11:05:09,270.339,0x0020,25.6,34265,0x001A,25,5347,5347,643,65535,0,0,0,201,25.3,2,100,89,38500,0,0x0282,0x0A,5347,3000,5347,0,0x00,0x0000,0x00,0x00,0,0,-273.2,0,0,0,0,0,0,0,0,0,0,0,0,564,SUCCESS

  • 您好, 数据上看刚开始充电RM就变成5347mAh, RSOC就到100%了

    请参考TRM 18页,所有的参数是否都scale

  • Hi Star,

    感谢回答 

    都 Scale 了还是出现一样的问题

    请教一下满充条件3. Voltage() is > ChargingVoltage() Taper Voltage

    这个Taper Voltage 是电芯电压还是pack电压?

  • 您好,taper voltage就是电压,不是电芯也不是pack,参数中能写入的最大值是1000mV

  • 11串应用. 单电芯充电电压是 3500mV, 所以 ChargingVoltage( ) 显示 38500mV

    Taper Voltage 设定 500mV

     Voltage() is > ChargingVoltage() – Taper Voltage

    请问满充条件是 38500mV-500mV 还是 38500mV-5500mV (500mVx11)

  • 您好,ChargingVoltage 是pack 电压,满充条件应该是38500mV-500mV

  • Hi Star,

    麻烦帮忙看一下gg, 都改了还是一样的情况

    34110_20220921.gg.csv

  • 您好,正常查询,稍后回复。

  • 您好,FC can be set in two ways, depending on the SOC Flag Configuration B (SOC Flag Config B) Register. 

    1-  If FCSETRSOC is set in (SOC Flag Config B) AND RSOC is greater or equal than FC_Set_RSOC, then FC = 1

    OR

    2-  If FCSetV is set in (SOC Flag Config B) AND cell voltage is greater than FC_set_voltage, then FC = 1


    Right now it looks like the customer has it configured by default, and neither are selected. Please see below

  • Hi Star,

    感谢回复,

    不过并没有解决问题

    就如回复的内容一样 SOC Flag Config B里面的

    FCSETRSOC=0, FCSETV=0, 这个是默认值没有问题吧?

    所以FC跳变到1的原因不是这2个设定

    不明白要我看SOC Flag Config B的目的是什么?

     

    在SOC Flag Config A里面已经是FCSETVCT=1

    问题是VCT的条件没到FC就=1了

  • 您好,上面发的内容提到FC设置有两种方式,请将FCSETRSOC=1, FCSETV=1

  • Hi Star,

    FCSETRSOC=1, FCSETV=1

    设定改了结果还是一样, 麻烦协助确认

    附上 log 及 gg

    Wed Sep 28 16:11:03 CST 2022
    
    Device Version Info = 0110_0_02
    BQZ Device Name = bq34110
    BQZ Firmware Version = 0_02
    
    Design Capacity = 6000
    
    Sample,DateTime,ElapsedTime,Control,Temperature,Voltage,Batt Stat,Current,RemCap,FullChgCap,AvgCurr,RunTimeEmty,AvgTimeFull,AccumulatedCharge,AccumulatedCharge Time,AvgPwr,IntTemp,CycleCnt,RSOC,SOH,ChgVolt,ChgCurr,OpStat,GaugeStat,CEDVRemCap,EDV Threshold,SmRemCap,SmCurrent,ManufacStat,EOSLearnStatus,EOSSafetyStatus,EOSStatus,AutoLearnTime,AvgDsgCurrent,AvgDsgTemp,LearnedResistance,LearnedResTimeHours,LearnedResTimeSeconds,LastLearnedResistance,LastLearnedResHours,LastLearnedResSeconds,InitialRRateAgeHours,InitialRRateAgeSeconds,RRate,RRateLong,InitialRcellRRateLearnRes,InitialRcellRRateLearnCount,LogRowTime(ms),LogStatus
    1,2022-09-28 16:11:08,5.011,0x0000,24.4,33396,0x4006,899,289,5347,555,65535,547,0,0,168,23.8,2,6,89,38500,6000,0x0282,0x04,289,0,288,0,0x00,0x0000,0x00,0x00,0,0,-273.2,0,0,0,0,0,0,0,0,0,0,0,0,568,SUCCESS
    2,2022-09-28 16:11:13,10.014,0x0000,24.4,33440,0x4006,899,290,5347,655,65535,463,0,0,199,23.9,2,6,89,38500,6000,0x0282,0x04,290,0,290,0,0x00,0x0000,0x00,0x00,0,0,-273.2,0,0,0,0,0,0,0,0,0,0,0,0,578,SUCCESS
    3,2022-09-28 16:11:18,15.017,0x0000,24.4,33484,0x4006,899,291,5347,726,65535,418,0,0,220,23.9,2,6,89,38500,6000,0x0282,0x04,291,0,291,0,0x00,0x0000,0x00,0x00,0,0,-273.2,0,0,0,0,0,0,0,0,0,0,0,0,561,SUCCESS
    4,2022-09-28 16:11:23,20.024,0x0000,24.4,33517,0x4006,899,292,5347,776,65535,391,0,0,236,23.9,2,6,89,38500,6000,0x0282,0x04,293,0,292,0,0x00,0x0000,0x00,0x00,0,0,-273.2,0,0,0,0,0,0,0,0,0,0,0,0,570,SUCCESS
    5,2022-09-28 16:11:28,25.025,0x0000,24.4,33561,0x4006,899,294,5347,812,65535,373,0,0,247,24.0,2,6,89,38500,6000,0x0282,0x04,294,0,293,0,0x00,0x0000,0x00,0x00,0,0,-273.2,0,0,0,0,0,0,0,0,0,0,0,0,584,SUCCESS
    6,2022-09-28 16:11:33,30.028,0x0000,24.4,33594,0x4006,899,295,5347,837,65535,362,0,0,255,24.0,2,6,89,38500,6000,0x0282,0x04,295,0,295,0,0x00,0x0000,0x00,0x00,0,0,-273.2,0,0,0,0,0,0,0,0,0,0,0,0,567,SUCCESS
    7,2022-09-28 16:11:38,35.038,0x0000,24.4,33627,0x4006,899,296,5347,855,65535,354,0,0,262,24.0,2,6,89,38500,6000,0x0282,0x04,296,0,296,0,0x00,0x0000,0x00,0x00,0,0,-273.2,0,0,0,0,0,0,0,0,0,0,0,0,586,SUCCESS
    8,2022-09-28 16:11:43,40.041,0x0000,24.4,33649,0x4006,899,297,5347,868,65535,349,0,0,265,24.1,2,6,89,38500,6000,0x0282,0x04,298,0,297,0,0x00,0x0000,0x00,0x00,0,0,-273.2,0,0,0,0,0,0,0,0,0,0,0,0,568,SUCCESS
    9,2022-09-28 16:11:48,45.045,0x0000,24.3,33682,0x4006,897,299,5347,877,65535,345,0,0,268,24.1,2,6,89,38500,6000,0x0282,0x04,299,0,298,0,0x00,0x0000,0x00,0x00,0,0,-273.2,0,0,0,0,0,0,0,0,0,0,0,0,565,SUCCESS
    10,2022-09-28 16:11:53,50.050,0x0000,24.3,33715,0x4006,897,300,5347,883,65535,343,0,0,270,24.1,2,6,89,38500,6000,0x0282,0x04,300,0,300,0,0x00,0x0000,0x00,0x00,0,0,-273.2,0,0,0,0,0,0,0,0,0,0,0,0,577,SUCCESS
    11,2022-09-28 16:11:58,55.052,0x0000,24.3,33737,0x4006,899,301,5347,888,65535,341,0,0,272,24.1,2,6,89,38500,6000,0x0282,0x04,301,0,301,0,0x00,0x0000,0x00,0x00,0,0,-273.2,0,0,0,0,0,0,0,0,0,0,0,0,573,SUCCESS
    12,2022-09-28 16:12:03,60.067,0x0000,24.3,33748,0x4006,899,302,5347,891,65535,340,0,0,273,24.1,2,6,89,38500,6000,0x0282,0x04,302,0,302,0,0x00,0x0000,0x00,0x00,0,0,-273.2,0,0,0,0,0,0,0,0,0,0,0,0,572,SUCCESS
    13,2022-09-28 16:12:08,65.075,0x0000,24.3,33781,0x4006,899,303,5347,893,65535,338,0,0,274,24.1,2,6,89,38500,6000,0x0282,0x04,304,0,303,0,0x00,0x0000,0x00,0x00,0,0,-273.2,0,0,0,0,0,0,0,0,0,0,0,0,568,SUCCESS
    14,2022-09-28 16:12:13,70.090,0x0000,24.3,33803,0x4006,899,305,5347,895,65535,0,0,0,275,24.2,2,100,89,38500,6000,0x0282,0x0A,5347,0,5347,0,0x00,0x0000,0x00,0x00,0,0,-273.2,0,0,0,0,0,0,0,0,0,0,0,0,564,SUCCESS
    15,2022-09-28 16:12:18,75.094,0x0000,24.3,33825,0x001A,899,5347,5347,896,65535,0,0,0,275,24.2,2,100,89,38500,0,0x0282,0x0A,5347,0,5347,0,0x00,0x0000,0x00,0x00,0,0,-273.2,0,0,0,0,0,0,0,0,0,0,0,0,563,SUCCESS
    16,2022-09-28 16:12:23,80.104,0x0000,24.3,33836,0x001A,897,5347,5347,897,65535,0,0,0,275,24.2,2,100,89,38500,0,0x0282,0x0A,5347,0,5347,0,0x00,0x0000,0x00,0x00,0,0,-273.2,0,0,0,0,0,0,0,0,0,0,0,0,570,SUCCESS
    

    20220928.gg.gg.csv

  • 您好,FCSETRSOC=1, FCSETV=1您选择一个置1,如果设置FCSETV=1,您看一下FC Set Voltage Threshold