This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

LM2611: 损坏

Part Number: LM2611

我们使用的LM2611芯片,在使用的时候偶尔会出现损坏的情况,供电电压9V,负载电流6mA。
检测供电端无高电压冲击。LM2611输出电压为-13.5V,后接LT1964,输出电压仍为-13.5V。
出现损坏概率很小,目前使用几百片,只出现了几片的损坏情况。
能帮分析一下芯片损坏原因吗?