This thread has been locked.
If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.
用这款充电芯片,当机器连接标充适配器充电时,打开机器上的打印头进行持续打印,过一段时间发现,关闭打印头后电池充电电流为0mA(这个是偶现的,不是每次都出现),充电器只会给系统供电,重启机器后现象依然存在。
请问是否能提供排查问题的建议?
谢谢!
出现充电电流为0mA的情况时,有打印log ,可以看到充电状态寄存器是0x03,是cc mode,充电使能标志位为1,充电器输出限制电流,充电电流,满电电压,设定都是正确的,vbus正确,vbat和vsys数值接近。
只有扣下电池再装回去后,再开机,才能正常充电,请问当充电电流为0mA时,充电芯片是不是进入了特定状态?
您好,现在vsys_min寄存器数值是7.0v,25度温度下电池放电100%对应的ocv电压对应6.8v多一点,会不会是vsys_min引起的,vsys_min是否要再设置小一些?
您好,Can you check all STAT and FLAG register readings? They are located from Reg 0x0B to 0x10. A spike in load(stop printing in your case) may have caused some fault conditions. Information from registers will give us more clue.
Also, when this happens, are you able to re-enable charging in software?
您好,由于是偶现,目前还在复现中。
请问能否大概推断一下charge ic哪方面异常会出现ibat为0mA?每次插上充电器软件都会enable一次charge ic。
您好,我们这边复现了,插着充电器时读取所有寄存器的值如下:
REG0:A0, REG1:4A, REG2:85, REG3:20, REG4:21
REG5:85, REG6:3D, REG7:A, REG8:D, REG9:15
REGa:0, REGb:3, REGc:80, REGd:0, REGe:0
REGf:0, REG10:80, REG11:0, REG12:0, REG13:0
REG14:0, REG15:B0, REG16:0, REG17:0, REG18:85
REG19:0, REG1a:0, REG1b:13, REG1c:6D, REG1d:1A
REG1e:6C, REG1f:1B, REG20:F2, REG21:2, REG22:8
REG23:0, REG24:3B, REG25:11
您好,设置看起来没有问题
However, device was not able to detect VBUS: Reg0C=80 and "Power good" was toggled, REG10=80, meaning some kind power reset was happening. Please check if anything triggered at customer input side, maybe power glitch for example.
建议您安装TI Battery management studio复现一下当时的现象, 手动输入registers的值, This will help expedite the real time debug,
您好,The EN_HIZ bit is cleared automatically when the adapter is plugged in.
请参考数据手册8.3.3.1 Poor Source Qualification确认是不是VBUS OVP引起的EN_HIZ