配置剩余容量RemCap lnit Percent为100%,左边状态栏显示只有9%~10%,是什么原因
This thread has been locked.
If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.
您好,The initial RC is estimated using the voltage characteristics of the programmed battery voltage table (see Voltage 0% DOD through
Voltage 100% DOD) and Learned Full Charge Capacity.详细请参考TRM 2.7.10 Initial Battery Capacity at Device Reset