This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

BQ28Z610: BQ28Z610 2串

Part Number: BQ28Z610
Other Parts Discussed in Thread: BQ40Z50-R1

    TI工程师好

   2串电池用BQ28Z610,用1个tssop-8的MOS和用两个tssop-8的MOS并联 ,过充保护后测试到的电压不一样;

   1、只用一个MOS,软件上显示电压为8.136V,用FLUKE测得电压和这一样;

    2、只用两个MOS并联,软件上显示电压为8.539V,用FLUKE测得电压为8.8V左右,电压是跳动的;

请问下为什么会这样,同一个板子只有加一个MOS就出现这个情况了。请帮忙分析下,

 谢谢!

  • 您好,能将电路发过来看一下吗?并联的MOS是哪个MOS

  • MOS管用的是AO8814

  • 您好,由于问题比较复杂,我需要询问更了解这款芯片的TI工程师,再帮您解答,稍后回复。

  • 您好 ,Usually it is only two N-Channel MOSFET in series back to back. I have never seen a design with parallel MOSFETs. Any particular reason for this?

    Parallel MOSFETs can cause imbalance in current during switching transitions if the wiring  layout of each MOSFETs are not identical. This can increase power losses. 

  • 1、1个MOS不满足工作电流就搞两个并联用,

    2、现在不是驱动不了的问题啊,是过充电保护了(XDSG置1),用的MOS数量越多,输出端的电压越高,MOS关不了?

    2、BQ40Z50-r1用3对MOS也没有这现象啊,

  • 您好,您的工作电流是多少,帮您查询一下。

  • 我是说用两个mos ,是因为产品工作电流1个mos不够的时候才用两个,

    然后为什么过充保护了就出现输出电压不对?

  • 您好 ,正在查询,稍后回复。

  • 您好,From the pictures above, I can only see few responses from the gauge. Do you have a log file which describes this scenario?

    I have couple of questions, from the schematic above I do not see any protector. If no protection is being used in the schematic, did you disable the protections under Settings: Enable Protections A and Settings:Enable Protections B?

    Can you share the log and gg file? 

  •  2S.gg.csv

    XCHG不是充电MOS管关闭了?

    gg文件已上传

  • 您好,From gg file, I can see that Overcurrent in Charge protection is enabled. From the above schematic, I do not see any protector. This is a problem, the gauge will act as if protectors are part of the system. 

    I suggest disabling the Overcurrent In Charge Protection if not protection is being used, or even disabling protections if not used at all. Or, increasing OCC:Threshold if current is greater than this threshold.

    I will need a log file to provide more details, but essentially if the current is greater than OCC:Threshold for OCC:Delay duration, this will trigger Overcurrent in Charge Protection. 

  • Fri Oct 28 05:34:50 GMT 2022
    
    Device Name = bq28z610
    Firmware Version = 0_17
    
    
    Sample,DateTime,ElapsedTime,ManufAccess,@Rate(@),@TimeEmpty,Temperature,Voltage,Current,AvgCurr,AvgPow,BTPDsgSet,BTPChgSet,RSOC,RemCap,FullChgCap,RunTimeEmty,AvgTimeFull,StandbyCurrent,StandbyTimeEmty,MaxLoadCurrent,MaxLoadTimeEmty,ChgCurr,ChgVolt,BattStat,CycleCnt,SoH,OpStatA,OpStatB,TempRange,ChgStat,GaugeStat,ITStat,MfgStat,SafetyAlertAB,SafetyStatAB,SafetyAlertCD,SafetyStatCD,PFAlertAB,PFStatAB,PFAlertCD,PFStatCD,CellVolt1,CellVolt2,vBAT,vPACK,CellCurr1,CellCurr2,CellPower1,CellPower2,Power,IntTemp,TS1Temp,CellTemp,FltRemQ,FltRemE,FltFullChgQ,FltFullChgE,NoLoadRemCap,TrueRemQ,TrueRemE,InitialQ,InitialE,TrueFullChgQ,TrueFullChgE,T_sim,T_ambient,RaScale1,RaScale2,CompRes1,CompRes2,PackGrid,LStatus,CellGrid1,CellGrid2,StateTime,DOD0_1,DOD0_2,DOD0 Passed Q,DOD0 Passed E,DOD0 Time,DODEOC_1,DODEOC_2,QMax1,QMax2,QMaxDOD0_1,QMaxDOD0_2,QMaxPassedQ,QMaxTime,Tk,Ta,RawDOD_1,RawDOD_2,CBTime1,CBTime2,CBDOD_1,CBDOD_2,CBTotalDODChg,LogRowTime(ms),LogStatus
    1,2022-10-28 05:34:54,4.000,0x0076,0,65535,27.6,8330,0,0,0,150,175,85,2356,2779,65535,65535,0,65535,-2000,71,2000,8700,0x00C0,3,96,0x0106,0x0000,0x08,0x0008,0x50,0x0814,0x0038,0x0000,0x0000,0x0000,0x0000,0x0000,0x0000,0x0000,0x0000,4165,4165,8333,8332,0,0,0,0,0,27.6,-53.5,27.6,2356,1775,2779,2130,0,2356,1775,423,355,2779,2130,27.6,27.4,1000,1000,0,0,0,14,0,0,64,2448,2432,0,0,0,0,0,2858,2849,0,0,0,0,3.76,3413,2448,2432,0,2056,2448,2432,16384,953,SUCCESS
    2,2022-10-28 05:34:58,8.000,0x0076,0,65535,29.1,8401,462,185,154,150,175,85,2356,2779,65535,129,0,65535,-2000,71,2000,8700,0x0080,3,96,0x0186,0x1000,0x08,0x0008,0x10,0x0814,0x0038,0x0000,0x0000,0x0000,0x0000,0x0000,0x0000,0x0000,0x0000,4202,4199,8403,8410,452,454,190,191,384,29.3,-53.3,29.3,2356,1774,2779,2129,0,2356,1774,423,355,2779,2129,27.6,27.4,1000,1000,0,0,0,14,0,0,3,2448,2432,0,0,0,0,0,2858,2849,0,0,0,0,3.76,3413,2448,2432,0,2053,2448,2432,16384,969,SUCCESS
    3,2022-10-28 05:35:02,12.000,0x0076,0,65535,29.9,8402,439,249,208,150,175,85,2357,2779,65535,103,0,65535,-2000,71,2000,8700,0x0080,3,96,0x0186,0x1000,0x08,0x0008,0x10,0x0814,0x0038,0x0000,0x0000,0x0000,0x0000,0x0000,0x0000,0x0000,0x0000,4203,4200,8405,8412,431,434,181,182,366,30.1,-53.4,30.1,2357,1774,2779,2129,0,2357,1774,423,355,2779,2129,27.6,27.4,1000,1000,0,0,0,14,0,0,7,2448,2432,-1,0,0,0,0,2858,2849,0,0,-1,0,3.76,3413,2448,2432,0,2049,2448,2432,16384,953,SUCCESS
    4,2022-10-28 05:35:06,16.000,0x0076,0,65535,30.3,8403,425,293,253,150,175,85,2357,2779,65535,99,0,65535,-2000,71,2000,8700,0x0080,3,96,0x0186,0x1000,0x08,0x0008,0x10,0x0814,0x0038,0x0000,0x0000,0x0000,0x0000,0x0000,0x0000,0x0000,0x0000,4203,4201,8406,8411,421,417,177,175,356,30.5,-53.4,30.5,2357,1774,2779,2129,0,2357,1774,423,355,2779,2129,27.6,27.4,1000,1000,0,0,0,14,0,0,11,2448,2432,-1,0,0,0,0,2858,2849,0,0,-1,0,3.76,3413,2448,2432,0,2045,2448,2432,16384,953,SUCCESS
    5,2022-10-28 05:35:10,20.000,0x0076,0,65535,30.6,8404,416,330,276,150,175,85,2358,2779,65535,93,0,65535,-2000,71,2000,8700,0x0080,3,96,0x0186,0x1000,0x08,0x0008,0x10,0x0814,0x0038,0x0000,0x0000,0x0000,0x0000,0x0000,0x0000,0x0000,0x0000,4203,4201,8405,8414,410,408,172,171,348,30.7,-53.5,30.7,2358,1775,2779,2129,0,2358,1775,423,355,2779,2129,27.6,27.4,1000,1000,0,0,0,14,0,0,15,2448,2432,-2,-1,0,0,0,2858,2849,0,0,-2,0,3.76,3413,2448,2432,0,2041,2448,2432,16384,953,SUCCESS
    6,2022-10-28 05:35:14,24.000,0x0076,0,65535,30.9,8405,407,349,293,150,175,85,2358,2779,65535,89,0,65535,-2000,71,2000,8700,0x0080,3,96,0x0186,0x1000,0x10,0x0008,0x10,0x0814,0x0038,0x0000,0x0000,0x0000,0x0000,0x0000,0x0000,0x0000,0x0000,4203,4201,8407,8414,404,404,170,170,341,30.9,-53.5,31.0,2358,1775,2779,2129,0,2358,1775,423,355,2779,2129,27.6,27.4,1000,1000,0,0,0,14,0,0,19,2448,2432,-2,-1,0,0,0,2858,2849,0,0,-2,0,3.76,3413,2448,2432,0,2037,2448,2432,16384,953,SUCCESS
    7,2022-10-28 05:35:18,28.000,0x0076,0,65535,31.1,8405,400,362,304,150,175,85,2359,2779,65535,87,0,65535,-2000,71,2000,8700,0x0080,3,96,0x0186,0x1000,0x10,0x0008,0x10,0x0814,0x0038,0x0000,0x0000,0x0000,0x0000,0x0000,0x0000,0x0000,0x0000,4203,4202,8407,8413,395,397,166,167,335,31.1,-53.4,31.2,2359,1776,2779,2129,0,2359,1776,423,355,2779,2129,27.6,27.4,1000,1000,0,0,0,14,0,0,23,2448,2432,-3,-2,0,0,0,2858,2849,0,0,-3,0,3.76,3413,2448,2432,0,2033,2448,2432,16384,953,SUCCESS
    8,2022-10-28 05:35:22,32.000,0x0076,0,65535,31.3,8406,393,370,310,150,175,85,2359,2779,65535,86,0,65535,-2000,71,2000,8700,0x0080,3,96,0x0186,0x1000,0x10,0x0008,0x10,0x0814,0x0038,0x0000,0x0000,0x0000,0x0000,0x0000,0x0000,0x0000,0x0000,4204,4202,8407,8414,390,388,164,163,330,31.3,-53.3,31.3,2359,1776,2779,2129,0,2359,1776,423,355,2779,2129,27.6,27.4,1000,1000,0,0,0,14,0,0,27,2448,2432,-3,-2,0,0,0,2858,2849,0,0,-3,0,3.76,3413,2448,2432,0,2029,2448,2432,16384,953,SUCCESS
    9,2022-10-28 05:35:26,36.000,0x0076,0,65535,31.4,8406,387,374,314,150,175,85,2359,2779,65535,85,0,65535,-2000,71,2000,8700,0x0080,3,96,0x0186,0x1000,0x10,0x0008,0x10,0x0814,0x0038,0x0000,0x0000,0x0000,0x0000,0x0000,0x0000,0x0000,0x0000,4205,4203,8408,8414,386,384,162,161,325,31.5,-53.5,31.5,2360,1777,2779,2129,0,2360,1777,423,355,2779,2129,27.6,27.4,1000,1000,0,0,0,14,0,0,31,2448,2432,-4,-3,0,0,0,2858,2849,0,0,-4,0,3.76,3413,2448,2432,0,2025,2448,2432,16384,953,SUCCESS
    10,2022-10-28 05:35:30,40.000,0x0076,0,65535,31.5,8407,381,376,316,150,175,85,2360,2779,65535,85,0,65535,-2000,71,2000,8700,0x0080,3,96,0x0186,0x1000,0x10,0x0008,0x10,0x0814,0x0038,0x0000,0x0000,0x0000,0x0000,0x0000,0x0000,0x0000,0x0000,4204,4203,8409,8414,380,380,160,160,320,31.5,-53.4,31.5,2360,1777,2779,2129,0,2360,1777,423,355,2779,2129,27.6,27.4,1000,1000,0,0,0,14,0,0,35,2448,2432,-4,-3,0,0,0,2858,2849,0,0,-4,0,3.76,3413,2448,2432,0,2021,2448,2432,16384,953,SUCCESS
    11,2022-10-28 05:35:34,44.000,0x0076,0,65535,31.6,8407,376,377,317,150,175,85,2360,2779,65535,85,0,65535,-2000,71,2000,8700,0x0080,3,96,0x0186,0x1000,0x10,0x0008,0x10,0x0814,0x0038,0x0000,0x0000,0x0000,0x0000,0x0000,0x0000,0x0000,0x0000,4205,4203,8409,8415,375,375,158,158,316,31.5,-53.4,31.5,2360,1777,2779,2129,0,2360,1777,423,355,2779,2129,27.6,27.4,1000,1000,0,0,0,14,0,0,39,2448,2432,-4,-3,0,0,0,2858,2849,0,0,-4,0,3.76,3413,2448,2432,0,2017,2448,2432,16384,953,SUCCESS
    12,2022-10-28 05:35:38,48.000,0x0076,0,65535,31.6,8407,371,376,316,150,175,85,2361,2779,65535,85,0,65535,-2000,71,2000,8700,0x0080,3,96,0x0186,0x1000,0x10,0x0008,0x10,0x0814,0x0038,0x0000,0x0000,0x0000,0x0000,0x0000,0x0000,0x0000,0x0000,4204,4203,8409,8414,369,370,155,156,312,31.6,-53.5,31.6,2361,1778,2779,2129,0,2361,1778,423,355,2779,2129,27.6,27.4,1000,1000,0,0,0,14,0,0,43,2448,2432,-5,-4,0,0,0,2858,2849,0,0,-5,0,3.76,3413,2448,2432,0,2013,2448,2432,16384,953,SUCCESS
    13,2022-10-28 05:35:42,52.000,0x0076,0,65535,31.6,8408,367,374,315,150,175,85,2361,2779,65535,85,0,65535,-2000,71,2000,8700,0x0080,3,96,0x0186,0x1000,0x10,0x0008,0x10,0x0814,0x0038,0x0000,0x0000,0x0000,0x0000,0x0000,0x0000,0x0000,0x0000,4205,4203,8409,8416,365,363,153,153,309,31.6,-53.3,31.6,2361,1778,2779,2129,0,2361,1778,423,355,2779,2129,27.6,27.4,1000,1000,0,0,0,14,0,0,47,2448,2432,-5,-4,0,0,0,2858,2849,0,0,-5,0,3.76,3413,2448,2432,0,2009,2448,2432,16384,953,SUCCESS
    14,2022-10-28 05:35:46,56.000,0x0076,0,65535,31.7,8408,363,372,313,150,175,85,2362,2779,65535,85,0,65535,-2000,71,2000,8700,0x0080,3,96,0x0186,0x1000,0x10,0x0008,0x10,0x0814,0x0038,0x0000,0x0000,0x0000,0x0000,0x0000,0x0000,0x0000,0x0000,4205,4203,8411,8414,361,358,152,150,304,31.7,-53.5,31.7,2362,1779,2779,2129,0,2362,1779,423,355,2779,2129,27.6,27.4,1000,1000,0,0,0,14,0,0,51,2448,2432,-6,-5,0,0,0,2858,2849,0,0,-6,0,3.76,3413,2448,2432,0,2005,2448,2432,16384,953,SUCCESS
    15,2022-10-28 05:35:50,60.000,0x0076,0,65535,31.7,8408,359,369,310,150,175,85,2362,2779,65535,86,0,65535,-2000,71,2000,8700,0x0080,3,96,0x0186,0x1000,0x10,0x0008,0x10,0x0814,0x0038,0x0000,0x0000,0x0000,0x0000,0x0000,0x0000,0x0000,0x0000,4205,4203,8409,8415,358,357,151,150,301,31.7,-53.5,31.7,2362,1779,2779,2129,0,2362,1779,423,355,2779,2129,27.6,27.4,1000,1000,0,0,0,14,0,0,55,2448,2432,-6,-5,0,0,0,2858,2849,0,0,-6,0,3.76,3413,2448,2432,0,2000,2448,2432,16384,953,SUCCESS
    16,2022-10-28 05:35:54,64.000,0x0076,0,65535,31.7,8408,356,366,308,150,175,85,2362,2779,65535,86,0,65535,-2000,71,2000,8700,0x0080,3,96,0x0186,0x1000,0x10,0x0008,0x10,0x0814,0x0038,0x0000,0x0000,0x0000,0x0000,0x0000,0x0000,0x0000,0x0000,4205,4204,8409,8417,354,352,149,148,299,31.7,-53.3,31.7,2362,1779,2779,2129,0,2363,1779,423,355,2779,2129,27.6,27.4,1000,1000,0,0,0,14,0,0,59,2448,2432,-7,-5,0,0,0,2858,2849,0,0,-7,0,3.76,3413,2448,2432,0,1996,2448,2432,16384,953,SUCCESS
    17,2022-10-28 05:35:58,68.000,0x0076,0,65535,31.8,8409,352,363,305,150,175,86,2363,2779,65535,86,0,65535,-2000,71,2000,8700,0x0080,3,96,0x0186,0x1000,0x10,0x0008,0x10,0x0814,0x0038,0x0000,0x0000,0x0000,0x0000,0x0000,0x0000,0x0000,0x0000,4205,4203,8411,8417,348,348,146,146,295,31.7,-53.3,31.7,2363,1779,2779,2129,0,2363,1779,423,355,2779,2129,27.6,27.4,1000,1000,0,0,0,14,0,0,63,2448,2432,-7,-5,0,0,0,2858,2849,0,0,-7,0,3.76,3413,2448,2432,0,1992,2448,2432,16384,953,SUCCESS
    18,2022-10-28 05:36:02,72.000,0x0076,0,65535,31.8,8409,348,360,302,150,175,86,2363,2779,65535,87,0,65535,-2000,71,2000,8700,0x0080,3,96,0x0186,0x1000,0x10,0x0008,0x10,0x0814,0x0038,0x0000,0x0000,0x0000,0x0000,0x0000,0x0000,0x0000,0x0000,4205,4204,8411,8416,345,347,145,146,293,31.8,-53.3,31.8,2363,1779,2779,2129,0,2363,1779,423,355,2779,2129,27.6,27.4,1000,1000,0,0,0,14,0,0,67,2448,2432,-7,-5,0,0,0,2858,2849,0,0,-7,0,3.76,3413,2448,2432,0,1988,2448,2432,16384,953,SUCCESS
    19,2022-10-28 05:36:06,76.000,0x0076,0,65535,31.9,8409,345,356,300,150,175,86,2364,2779,65535,87,0,65535,-2000,71,2000,8700,0x0080,3,96,0x0186,0x1000,0x10,0x0008,0x10,0x0814,0x0038,0x0000,0x0000,0x0000,0x0000,0x0000,0x0000,0x0000,0x0000,4206,4204,8411,8416,341,342,143,144,289,31.9,-53.5,31.8,2364,1780,2779,2129,0,2364,1780,423,355,2779,2129,27.6,27.4,1000,1000,0,0,0,14,0,0,71,2448,2432,-8,-6,0,0,0,2858,2849,0,0,-8,0,3.76,3413,2448,2432,0,1984,2448,2432,16384,953,SUCCESS
    20,2022-10-28 05:36:10,80.000,0x0076,0,65535,31.9,8411,341,353,297,150,175,86,2364,2779,65535,88,0,65535,-2000,71,2000,8700,0x0080,3,96,0x0186,0x1000,0x10,0x0008,0x10,0x0814,0x0038,0x0000,0x0000,0x0000,0x0000,0x0000,0x0000,0x0000,0x0000,4206,4204,8411,8417,338,339,142,143,286,31.9,-53.4,31.9,2364,1780,2779,2129,0,2364,1780,423,355,2779,2129,27.6,27.4,1000,1000,0,0,0,14,0,0,76,2448,2432,-8,-6,0,0,0,2858,2849,0,0,-8,0,3.76,3413,2448,2432,0,1980,2448,2432,16384,953,SUCCESS
    21,2022-10-28 05:36:14,84.000,0x0076,0,65535,31.9,8411,338,350,294,150,175,86,2364,2779,65535,88,0,65535,-2000,71,2000,8700,0x0080,3,96,0x0186,0x1000,0x10,0x0008,0x10,0x0814,0x0038,0x0000,0x0000,0x0000,0x0000,0x0000,0x0000,0x0000,0x0000,4205,4204,8412,8417,335,335,141,141,284,31.9,-53.3,31.9,2364,1780,2779,2129,0,2364,1780,423,355,2779,2129,27.6,27.4,1000,1000,0,0,0,14,0,0,80,2448,2432,-8,-6,0,0,0,2858,2849,0,0,-8,0,3.76,3413,2448,2432,0,1976,2448,2432,16384,953,SUCCESS
    22,2022-10-28 05:36:18,88.000,0x0076,0,65535,31.9,8410,335,347,291,150,175,86,2365,2779,65535,89,0,65535,-2000,71,2000,8700,0x0080,3,96,0x0186,0x1000,0x10,0x0008,0x10,0x0814,0x0038,0x0000,0x0000,0x0000,0x0000,0x0000,0x0000,0x0000,0x0000,4206,4204,8412,8417,332,331,140,139,282,31.9,-53.4,31.9,2365,1781,2779,2129,0,2365,1781,423,355,2779,2129,27.6,27.4,1000,1000,0,0,0,14,0,0,84,2448,2432,-9,-7,0,0,0,2858,2849,0,0,-9,0,3.76,3413,2448,2432,0,1972,2448,2432,16384,953,SUCCESS
    23,2022-10-28 05:36:22,92.000,0x0076,0,65535,32.0,8411,331,343,289,150,175,86,2365,2779,65535,89,0,65535,-2000,71,2000,8700,0x0080,3,96,0x0186,0x1000,0x10,0x0008,0x10,0x0814,0x0038,0x0000,0x0000,0x0000,0x0000,0x0000,0x0000,0x0000,0x0000,4206,4204,8411,8418,330,330,139,139,278,32.0,-53.5,32.0,2365,1781,2779,2129,0,2365,1781,423,355,2779,2129,27.6,27.4,1000,1000,0,0,0,14,0,0,88,2448,2432,-9,-7,0,0,0,2858,2849,0,0,-9,0,3.76,3413,2448,2432,0,1968,2448,2432,16384,969,SUCCESS
    24,2022-10-28 05:36:26,96.000,0x0076,0,65535,31.9,8411,329,340,286,150,175,86,2365,2779,65535,90,0,65535,-2000,71,2000,8700,0x0080,3,96,0x0186,0x1000,0x10,0x0008,0x10,0x0814,0x0038,0x0000,0x0000,0x0000,0x0000,0x0000,0x0000,0x0000,0x0000,4206,4205,8412,8417,329,326,138,137,277,31.9,-53.5,31.9,2365,1782,2779,2129,0,2366,1782,423,355,2779,2129,27.6,27.4,1000,1000,0,0,0,14,0,0,92,2448,2432,-10,-8,0,0,0,2858,2849,0,0,-10,0,3.76,3413,2448,2432,0,1964,2448,2432,16384,969,SUCCESS
    25,2022-10-28 05:36:30,100.000,0x0076,0,65535,32.0,8411,326,337,283,150,175,86,2366,2779,65535,90,0,65535,-2000,71,2000,8700,0x0080,3,96,0x0186,0x1000,0x10,0x0008,0x10,0x0814,0x0038,0x0000,0x0000,0x0000,0x0000,0x0000,0x0000,0x0000,0x0000,4207,4205,8412,8418,324,323,136,136,274,32.0,-53.4,32.0,2366,1782,2779,2129,0,2366,1782,423,355,2779,2129,27.6,27.4,1000,1000,0,0,0,14,0,0,96,2448,2432,-10,-8,0,0,0,2858,2849,0,0,-10,0,3.76,3413,2448,2432,0,1960,2448,2432,16384,969,SUCCESS
    26,2022-10-28 05:36:34,104.000,0x0076,0,65535,32.0,8411,324,334,281,150,175,86,2366,2779,65535,91,0,65535,-2000,71,2000,8700,0x0080,3,96,0x0186,0x1000,0x10,0x0008,0x10,0x0814,0x0038,0x0000,0x0000,0x0000,0x0000,0x0000,0x0000,0x0000,0x0000,4206,4205,8414,8418,322,322,135,135,273,32.0,-53.4,32.0,2366,1782,2779,2129,0,2366,1782,423,355,2779,2129,27.6,27.4,1000,1000,0,0,0,14,0,0,100,2448,2432,-10,-8,0,0,0,2858,2849,0,0,-10,0,3.76,3413,2448,2432,0,1956,2448,2432,16384,969,SUCCESS
    27,2022-10-28 05:36:38,108.000,0x0076,0,65535,32.0,8411,321,331,278,150,175,86,2366,2779,65535,91,0,65535,-2000,71,2000,8700,0x0080,3,96,0x0186,0x1000,0x10,0x0008,0x10,0x0814,0x0038,0x0000,0x0000,0x0000,0x0000,0x0000,0x0000,0x0000,0x0000,4206,4205,8413,8416,318,317,134,133,270,32.0,-53.4,32.0,2367,1783,2779,2129,0,2367,1783,423,355,2779,2129,27.6,27.4,1000,1000,0,0,0,14,0,0,104,2448,2432,-11,-9,0,0,0,2858,2849,0,0,-11,0,3.76,3413,2448,2432,0,1952,2448,2432,16384,969,SUCCESS
    28,2022-10-28 05:36:42,112.000,0x0076,0,65535,32.0,8412,319,328,276,150,175,86,2367,2779,65535,92,0,65535,-2000,71,2000,8700,0x0080,3,96,0x0186,0x1000,0x10,0x0008,0x10,0x0814,0x0038,0x0000,0x0000,0x0000,0x0000,0x0000,0x0000,0x0000,0x0000,4206,4204,8411,8419,316,317,133,133,268,32.0,-53.5,32.0,2367,1783,2779,2129,0,2367,1783,423,355,2779,2129,27.6,27.4,1000,1000,0,0,0,14,0,0,108,2448,2432,-11,-9,0,0,0,2858,2849,0,0,-11,0,3.76,3413,2448,2432,0,1948,2448,2432,16384,969,SUCCESS
    29,2022-10-28 05:36:46,116.000,0x0076,0,65535,32.0,8412,316,326,274,150,175,86,2367,2779,65535,92,0,65535,-2000,71,2000,8700,0x0080,3,96,0x0186,0x1000,0x10,0x0008,0x10,0x0814,0x0038,0x0000,0x0000,0x0000,0x0000,0x0000,0x0000,0x0000,0x0000,4206,4204,8414,8420,313,314,132,132,266,32.1,-53.4,32.1,2367,1783,2779,2129,0,2367,1783,423,355,2779,2129,27.6,27.4,1000,1000,0,0,0,14,0,0,112,2448,2432,-11,-9,0,0,0,2858,2849,0,0,-11,0,3.76,3413,2448,2432,0,1944,2448,2432,16384,953,SUCCESS
    30,2022-10-28 05:36:50,120.000,0x0076,0,65535,32.0,8412,314,323,272,150,175,86,2368,2779,65535,92,0,65535,-2000,71,2000,8700,0x0080,3,96,0x0186,0x1000,0x10,0x0008,0x10,0x0814,0x0038,0x0000,0x0000,0x0000,0x0000,0x0000,0x0000,0x0000,0x0000,4207,4205,8414,8417,310,310,130,130,263,32.0,-53.5,32.0,2368,1784,2779,2129,0,2368,1784,423,355,2779,2129,27.6,27.4,1000,1000,0,0,0,14,0,0,116,2448,2432,-12,-10,0,0,0,2858,2849,0,0,-12,0,3.76,3413,2448,2432,0,1940,2448,2432,16384,969,SUCCESS
    31,2022-10-28 05:36:54,124.000,0x0076,0,65535,32.1,8412,312,321,270,150,175,86,2368,2779,65535,93,0,65535,-2000,71,2000,8700,0x0080,3,96,0x0186,0x1000,0x10,0x0008,0x10,0x0814,0x0038,0x0000,0x0000,0x0000,0x0000,0x0000,0x0000,0x0000,0x0000,4207,4205,8412,8417,310,306,130,129,262,32.1,-53.3,32.1,2368,1784,2779,2129,0,2368,1784,423,355,2779,2129,27.6,27.4,1000,1000,0,0,0,14,0,0,120,2448,2432,-12,-10,0,0,0,2858,2849,0,0,-12,0,3.76,3413,2448,2432,0,1936,2448,2432,16384,969,SUCCESS
    32,2022-10-28 05:36:58,128.000,0x0076,0,65535,32.1,8413,309,318,268,150,175,86,2368,2779,65535,93,0,65535,-2000,71,2000,8700,0x0080,3,96,0x0186,0x1000,0x10,0x0008,0x10,0x0814,0x0038,0x0000,0x0000,0x0000,0x0000,0x0000,0x0000,0x0000,0x0000,4207,4205,8413,8419,308,305,130,128,260,32.2,-53.4,32.2,2368,1784,2779,2129,0,2368,1784,423,355,2779,2129,27.6,27.4,1000,1000,0,0,0,14,0,0,124,2448,2432,-12,-10,0,0,0,2858,2849,0,0,-12,0,3.76,3413,2448,2432,0,1932,2448,2432,16384,969,SUCCESS
    33,2022-10-28 05:37:02,132.000,0x0076,0,65535,32.2,8413,307,316,265,150,175,86,2369,2779,65535,94,0,65535,-2000,71,2000,8700,0x0080,3,96,0x0186,0x1000,0x10,0x0008,0x10,0x0814,0x0038,0x0000,0x0000,0x0000,0x0000,0x0000,0x0000,0x0000,0x0000,4207,4205,8413,8418,304,302,128,127,257,32.2,-53.5,32.2,2369,1784,2779,2129,0,2369,1784,423,355,2779,2129,27.6,27.4,1000,1000,0,0,0,14,0,0,128,2448,2432,-13,-10,0,0,0,2858,2849,0,0,-13,0,3.76,3413,2448,2432,0,1928,2448,2432,16384,969,SUCCESS
    34,2022-10-28 05:37:06,136.000,0x0076,0,65535,32.2,8413,304,313,263,150,175,86,2369,2779,65535,94,0,65535,-2000,71,2000,8700,0x0080,3,96,0x0186,0x1000,0x10,0x0008,0x10,0x0814,0x0038,0x0000,0x0000,0x0000,0x0000,0x0000,0x0000,0x0000,0x0000,4207,4205,8413,8418,301,300,127,126,256,32.2,-53.3,32.2,2369,1784,2779,2129,0,2369,1784,423,355,2779,2129,27.6,27.4,1000,1000,0,0,0,14,0,0,132,2448,2432,-13,-10,0,0,0,2858,2849,0,0,-13,0,3.76,3413,2448,2432,0,1924,2448,2432,16384,969,SUCCESS
    35,2022-10-28 05:37:10,140.000,0x0076,0,65535,32.2,8412,302,311,261,150,175,86,2369,2779,65535,95,0,65535,-2000,71,2000,8700,0x0080,3,96,0x0186,0x1000,0x10,0x0008,0x10,0x0814,0x0038,0x0000,0x0000,0x0000,0x0000,0x0000,0x0000,0x0000,0x0000,4207,4205,8415,8418,299,298,126,125,254,32.2,-53.5,32.2,2369,1784,2779,2129,0,2369,1784,423,355,2779,2129,27.6,27.4,1000,1000,0,0,0,14,0,0,136,2448,2432,-13,-10,0,0,0,2858,2849,0,0,-13,0,3.76,3413,2448,2432,0,1920,2448,2432,16384,969,SUCCESS
    36,2022-10-28 05:37:14,144.000,0x0076,0,65535,32.2,8412,300,308,259,150,175,86,2370,2779,65535,95,0,65535,-2000,71,2000,8700,0x0080,3,96,0x0186,0x1000,0x10,0x0008,0x10,0x0814,0x0038,0x0000,0x0000,0x0000,0x0000,0x0000,0x0000,0x0000,0x0000,4207,4205,8415,8418,297,297,125,125,252,32.3,-53.4,32.2,2370,1785,2779,2129,0,2370,1785,423,355,2779,2129,27.6,27.4,1000,1000,0,0,0,14,0,0,140,2448,2432,-14,-11,0,0,0,2858,2849,0,0,-14,0,3.76,3413,2448,2432,0,1916,2448,2432,16384,969,SUCCESS
    37,2022-10-28 05:37:18,148.000,0x0076,0,65535,32.3,8412,298,306,258,150,175,86,2370,2779,65535,95,0,65535,-2000,71,2000,8700,0x0080,3,96,0x0186,0x1000,0x10,0x0008,0x10,0x0814,0x0038,0x0000,0x0000,0x0000,0x0000,0x0000,0x0000,0x0000,0x0000,4207,4205,8413,8419,296,295,125,124,251,32.3,-53.5,32.3,2370,1785,2779,2129,0,2370,1785,423,355,2779,2129,27.6,27.4,1000,1000,0,0,0,14,0,0,144,2448,2432,-14,-11,0,0,0,2858,2849,0,0,-14,0,3.76,3413,2448,2432,0,1912,2448,2432,16384,969,SUCCESS
    38,2022-10-28 05:37:22,152.000,0x0076,0,65535,32.3,8412,296,304,256,150,175,86,2370,2779,65535,96,0,65535,-2000,71,2000,8700,0x0080,3,96,0x0186,0x1000,0x10,0x0008,0x10,0x0814,0x0038,0x0000,0x0000,0x0000,0x0000,0x0000,0x0000,0x0000,0x0000,4207,4205,8414,8420,294,291,124,122,249,32.3,-53.4,32.3,2370,1785,2779,2129,0,2370,1785,423,355,2779,2129,27.6,27.4,1000,1000,0,0,0,14,0,0,148,2448,2432,-14,-11,0,0,0,2858,2849,0,0,-14,0,3.76,3413,2448,2432,0,1908,2448,2432,16384,969,SUCCESS
    39,2022-10-28 05:37:26,156.000,0x0076,0,65535,32.3,8413,294,302,254,150,175,86,2371,2779,65535,96,0,65535,-2000,71,2000,8700,0x0080,3,96,0x0186,0x1000,0x10,0x0008,0x10,0x0814,0x0038,0x0000,0x0000,0x0000,0x0000,0x0000,0x0000,0x0000,0x0000,4208,4205,8415,8419,292,290,123,122,247,32.3,-53.5,32.3,2371,1786,2779,2129,0,2371,1786,423,355,2779,2129,27.6,27.4,1000,1000,0,0,0,14,0,0,152,2448,2432,-15,-12,0,0,0,2858,2849,0,0,-15,0,3.76,3413,2448,2432,0,1904,2448,2432,16384,969,SUCCESS
    40,2022-10-28 05:37:30,160.000,0x0076,0,65535,32.3,8412,292,300,252,150,175,86,2371,2779,65535,97,0,65535,-2000,71,2000,8700,0x0080,3,96,0x0186,0x1000,0x10,0x0008,0x10,0x0814,0x0038,0x0000,0x0000,0x0000,0x0000,0x0000,0x0000,0x0000,0x0000,4208,4205,8413,8418,292,288,123,121,246,32.3,-53.5,32.3,2371,1786,2779,2129,0,2371,1786,423,355,2779,2129,27.6,27.4,1000,1000,0,0,0,14,0,0,156,2448,2432,-15,-12,0,0,0,2858,2849,0,0,-15,0,3.76,3413,2448,2432,0,1900,2448,2432,16384,969,SUCCESS
    41,2022-10-28 05:37:34,164.000,0x0076,0,65535,32.3,8413,290,298,251,150,175,86,2371,2779,65535,90,0,65535,-2000,71,2000,8700,0x0080,3,96,0x0186,0x1000,0x10,0x0008,0x10,0x0814,0x0038,0x0000,0x0000,0x0000,0x0000,0x0000,0x0000,0x0000,0x0000,4208,4206,8415,8420,289,287,122,121,244,32.4,-53.4,32.3,2371,1786,2779,2129,0,2371,1786,423,355,2779,2129,27.6,27.4,1000,1000,0,0,0,14,0,0,160,2448,2432,-15,-12,1,0,0,2858,2849,0,0,-15,1,3.76,3413,2448,2432,0,1896,2448,2432,16384,953,SUCCESS
    42,2022-10-28 05:37:38,168.000,0x0076,0,65535,32.3,8413,288,296,249,150,175,86,2372,2779,65535,90,0,65535,-2000,71,2000,8700,0x0080,3,96,0x0186,0x1000,0x10,0x0008,0x10,0x0814,0x0038,0x0000,0x0000,0x0000,0x0000,0x0000,0x0000,0x0000,0x0000,4208,4206,8415,8420,287,285,121,120,242,32.4,-53.3,32.3,2372,1787,2779,2129,0,2372,1787,423,355,2779,2129,27.6,27.4,1000,1000,0,0,0,14,0,0,164,2448,2432,-16,-13,1,0,0,2858,2849,0,0,-16,1,3.76,3413,2448,2432,0,1892,2448,2432,16384,969,SUCCESS
    43,2022-10-28 05:37:42,172.000,0x0076,0,65535,32.3,8412,286,294,247,150,175,86,2372,2779,65535,90,0,65535,-2000,71,2000,8700,0x0080,3,96,0x0186,0x1000,0x10,0x0008,0x10,0x0814,0x0038,0x0000,0x0000,0x0000,0x0000,0x0000,0x0000,0x0000,0x0000,4208,4205,8415,8419,286,284,120,119,241,32.3,-53.3,32.3,2372,1787,2779,2129,0,2372,1787,423,355,2779,2129,27.6,27.4,1000,1000,0,0,0,14,0,0,168,2448,2432,-16,-13,1,0,0,2858,2849,0,0,-16,1,3.76,3413,2448,2432,0,1888,2448,2432,16384,953,SUCCESS
    44,2022-10-28 05:37:46,176.000,0x0076,0,65535,32.3,8413,284,292,246,150,175,86,2372,2779,65535,91,0,65535,-2000,71,2000,8700,0x0080,3,96,0x0186,0x1000,0x10,0x0008,0x10,0x0814,0x0038,0x0000,0x0000,0x0000,0x0000,0x0000,0x0000,0x0000,0x0000,4208,4206,8415,8419,283,280,119,118,239,32.4,-53.4,32.4,2372,1787,2779,2129,0,2372,1787,423,355,2779,2129,27.6,27.4,1000,1000,0,0,0,14,0,0,172,2448,2432,-16,-13,1,0,0,2858,2849,0,0,-16,1,3.76,3413,2448,2432,0,1884,2448,2432,16384,953,SUCCESS
    45,2022-10-28 05:37:50,180.000,0x0076,0,65535,32.3,8413,282,290,244,150,175,86,2372,2779,65535,91,0,65535,-2000,71,2000,8700,0x0080,3,96,0x0186,0x1000,0x10,0x0008,0x10,0x0814,0x0038,0x0000,0x0000,0x0000,0x0000,0x0000,0x0000,0x0000,0x0000,4208,4205,8415,8419,280,279,118,117,237,32.4,-53.4,32.4,2373,1788,2779,2129,0,2373,1788,423,355,2779,2129,27.6,27.4,1000,1000,0,0,0,14,0,0,176,2448,2432,-17,-14,1,0,0,2858,2849,0,0,-17,1,3.76,3413,2448,2432,0,1880,2448,2432,16384,953,SUCCESS
    46,2022-10-28 05:37:54,184.000,0x0076,0,65535,32.3,8414,281,288,242,150,175,86,2373,2779,65535,92,0,65535,-2000,71,2000,8700,0x0080,3,96,0x0186,0x1000,0x10,0x0008,0x10,0x0814,0x0038,0x0000,0x0000,0x0000,0x0000,0x0000,0x0000,0x0000,0x0000,4210,4205,8415,8420,277,279,117,117,236,32.3,-53.5,32.3,2373,1788,2779,2129,0,2373,1788,423,355,2779,2129,27.6,27.4,1000,1000,0,0,0,14,0,0,180,2448,2432,-17,-14,1,0,0,2858,2849,0,0,-17,1,3.76,3413,2448,2432,0,1876,2448,2432,16384,969,SUCCESS
    47,2022-10-28 05:37:58,188.000,0x0076,0,65535,32.3,8413,279,286,241,150,175,86,2373,2779,65535,92,0,65535,-2000,71,2000,8700,0x0080,3,96,0x0186,0x1000,0x10,0x0008,0x10,0x0814,0x0038,0x0000,0x0000,0x0000,0x0000,0x0000,0x0000,0x0000,0x0000,4210,4206,8416,8420,279,278,117,117,235,32.3,-53.5,32.3,2373,1788,2779,2129,0,2373,1788,423,355,2779,2129,27.6,27.4,1000,1000,0,0,0,14,0,0,184,2448,2432,-17,-14,1,0,0,2858,2849,0,0,-17,1,3.76,3413,2448,2432,0,1872,2448,2432,16384,969,SUCCESS
    48,2022-10-28 05:38:02,192.000,0x0076,0,65535,32.2,8414,278,284,239,150,175,86,2373,2779,65535,93,0,65535,-2000,71,2000,8700,0x0080,3,96,0x0186,0x1000,0x10,0x0008,0x10,0x0814,0x0038,0x0000,0x0000,0x0000,0x0000,0x0000,0x0000,0x0000,0x0000,4209,4205,8415,8420,274,274,115,115,234,32.2,-53.3,32.3,2374,1789,2779,2129,0,2374,1789,423,355,2779,2129,27.6,27.4,1000,1000,0,0,0,14,0,0,188,2448,2432,-18,-15,1,0,0,2858,2849,0,0,-18,1,3.76,3413,2448,2432,0,1868,2448,2432,16384,969,SUCCESS
    49,2022-10-28 05:38:06,196.000,0x0076,0,65535,32.2,8414,276,283,238,150,175,86,2374,2779,65535,93,0,65535,-2000,71,2000,8700,0x0080,3,96,0x0186,0x1000,0x10,0x0008,0x10,0x0814,0x0038,0x0000,0x0000,0x0000,0x0000,0x0000,0x0000,0x0000,0x0000,4209,4206,8415,8419,274,272,115,114,232,32.2,-53.4,32.3,2374,1789,2779,2129,0,2374,1789,423,355,2779,2129,27.6,27.4,1000,1000,0,0,0,14,0,0,192,2448,2432,-18,-15,1,0,0,2858,2849,0,0,-18,1,3.76,3413,2448,2432,0,1864,2448,2432,16384,969,SUCCESS
    50,2022-10-28 05:38:10,200.000,0x0076,0,65535,32.2,8414,274,281,236,150,175,86,2374,2779,65535,93,0,65535,-2000,71,2000,8700,0x0080,3,96,0x0186,0x1000,0x10,0x0008,0x10,0x0814,0x0038,0x0000,0x0000,0x0000,0x0000,0x0000,0x0000,0x0000,0x0000,4209,4205,8415,8420,273,271,115,114,231,32.2,-53.4,32.2,2374,1789,2779,2129,0,2374,1789,423,355,2779,2129,27.6,27.4,1000,1000,0,0,0,14,0,0,196,2448,2432,-18,-15,1,0,0,2858,2849,0,0,-18,1,3.76,3413,2448,2432,0,1860,2448,2432,16384,953,SUCCESS
    51,2022-10-28 05:38:14,204.000,0x0076,0,65535,32.2,8414,273,279,235,150,175,86,2374,2779,65535,94,0,65535,-2000,71,2000,8700,0x0080,3,96,0x0186,0x1000,0x10,0x0008,0x10,0x0814,0x0038,0x0000,0x0000,0x0000,0x0000,0x0000,0x0000,0x0000,0x0000,4209,4205,8415,8419,270,271,114,114,230,32.2,-53.4,32.2,2374,1789,2779,2129,0,2375,1789,423,355,2779,2129,27.6,27.4,1000,1000,0,0,0,14,0,0,200,2448,2432,-19,-15,1,0,0,2858,2849,0,0,-19,1,3.76,3413,2448,2432,0,1856,2448,2432,16384,969,SUCCESS
    52,2022-10-28 05:38:18,208.000,0x0076,0,65535,32.2,8414,271,277,234,150,175,86,2375,2779,65535,94,0,65535,-2000,71,2000,8700,0x0080,3,96,0x0186,0x1000,0x10,0x0008,0x10,0x0814,0x0038,0x0000,0x0000,0x0000,0x0000,0x0000,0x0000,0x0000,0x0000,4209,4205,8415,8420,271,269,114,113,228,32.2,-53.3,32.2,2375,1789,2779,2129,0,2375,1789,423,355,2779,2129,27.6,27.4,1000,1000,0,0,0,14,0,0,204,2448,2432,-19,-15,1,0,0,2858,2849,0,0,-19,1,3.76,3413,2448,2432,0,1852,2448,2432,16384,969,SUCCESS
    53,2022-10-28 05:38:22,212.000,0x0076,0,65535,32.3,8414,270,276,232,150,175,86,2375,2779,65535,95,0,65535,-2000,71,2000,8700,0x0080,3,96,0x0186,0x1000,0x10,0x0008,0x10,0x0814,0x0038,0x0000,0x0000,0x0000,0x0000,0x0000,0x0000,0x0000,0x0000,4210,4206,8417,8419,268,269,113,113,226,32.2,-53.4,32.2,2375,1789,2779,2129,0,2375,1789,423,355,2779,2129,27.6,27.4,1000,1000,0,0,0,14,0,0,208,2448,2432,-19,-15,1,0,0,2858,2849,0,0,-19,1,3.76,3413,2448,2432,0,1848,2448,2432,16384,953,SUCCESS
    54,2022-10-28 05:38:26,216.000,0x0076,0,65535,32.3,8414,268,274,231,150,175,86,2375,2779,65535,95,0,65535,-2000,71,2000,8700,0x0080,3,96,0x0186,0x1000,0x10,0x0008,0x10,0x0814,0x0038,0x0000,0x0000,0x0000,0x0000,0x0000,0x0000,0x0000,0x0000,4210,4205,8415,8420,265,268,112,113,226,32.2,-53.4,32.2,2375,1789,2779,2129,0,2375,1789,423,355,2779,2129,27.6,27.4,1000,1000,0,0,0,14,0,0,212,2448,2432,-19,-15,1,0,0,2858,2849,0,0,-19,1,3.76,3413,2448,2432,0,1844,2448,2432,16384,969,SUCCESS
    55,2022-10-28 05:38:30,220.000,0x0076,0,65535,32.3,8415,267,272,229,150,175,86,2376,2779,65535,96,0,65535,-2000,71,2000,8700,0x0080,3,96,0x0186,0x1000,0x10,0x0008,0x10,0x0814,0x0038,0x0000,0x0000,0x0000,0x0000,0x0000,0x0000,0x0000,0x0000,4210,4205,8415,8422,265,264,112,111,224,32.3,-53.3,32.2,2376,1790,2779,2129,0,2376,1790,423,355,2779,2129,27.6,27.4,1000,1000,0,0,0,14,0,0,216,2448,2432,-20,-16,1,0,0,2858,2849,0,0,-20,1,3.76,3413,2448,2432,0,1840,2448,2432,16384,969,SUCCESS
    56,2022-10-28 05:38:34,224.000,0x0076,0,65535,32.2,8415,265,271,228,150,175,86,2376,2779,65535,96,0,65535,-2000,71,2000,8700,0x0080,3,96,0x0186,0x1000,0x10,0x0008,0x10,0x0814,0x0038,0x0000,0x0000,0x0000,0x0000,0x0000,0x0000,0x0000,0x0000,4210,4206,8417,8419,264,262,111,110,222,32.2,-53.4,32.2,2376,1790,2779,2129,0,2376,1790,423,355,2779,2129,27.6,27.4,1000,1000,0,0,0,14,0,0,220,2448,2432,-20,-16,1,0,0,2858,2849,0,0,-20,1,3.76,3413,2448,2432,0,1836,2448,2432,16384,969,SUCCESS
    57,2022-10-28 05:38:38,228.000,0x0076,0,65535,32.2,8415,264,269,227,150,175,86,2376,2779,65535,96,0,65535,-2000,71,2000,8700,0x0080,3,96,0x0186,0x1000,0x10,0x0008,0x10,0x0814,0x0038,0x0000,0x0000,0x0000,0x0000,0x0000,0x0000,0x0000,0x0000,4210,4205,8415,8420,260,262,109,110,222,32.2,-53.4,32.2,2376,1790,2779,2129,0,2376,1790,423,355,2779,2129,27.6,27.4,1000,1000,0,0,0,14,0,0,224,2448,2432,-20,-16,1,0,0,2858,2849,0,0,-20,1,3.76,3413,2448,2432,0,1832,2448,2432,16384,969,SUCCESS
    58,2022-10-28 05:38:42,232.000,0x0076,0,65535,32.2,8414,262,268,225,150,175,86,2376,2779,65535,97,0,65535,-2000,71,2000,8700,0x0080,3,96,0x0186,0x1000,0x10,0x0008,0x10,0x0814,0x0038,0x0000,0x0000,0x0000,0x0000,0x0000,0x0000,0x0000,0x0000,4210,4206,8416,8421,259,259,109,109,220,32.3,-53.5,32.3,2377,1791,2779,2129,0,2377,1791,423,355,2779,2129,27.6,27.4,1000,1000,0,0,0,14,0,0,228,2448,2432,-21,-17,1,0,0,2858,2849,0,0,-21,1,3.76,3413,2448,2432,0,1828,2448,2432,16384,969,SUCCESS
    59,2022-10-28 05:38:46,236.000,0x0076,0,65535,32.2,8415,260,266,224,150,175,86,2377,2779,65535,97,0,65535,-2000,71,2000,8700,0x0080,3,96,0x0186,0x1000,0x10,0x0008,0x10,0x0814,0x0038,0x0000,0x0000,0x0000,0x0000,0x0000,0x0000,0x0000,0x0000,4210,4206,8417,8420,256,257,108,108,219,32.2,-53.4,32.2,2377,1791,2779,2129,0,2377,1791,423,355,2779,2129,27.6,27.4,1000,1000,0,0,0,14,0,0,232,2448,2432,-21,-17,1,0,0,2858,2849,0,0,-21,1,3.76,3413,2448,2432,0,1824,2448,2432,16384,953,SUCCESS
    60,2022-10-28 05:38:50,240.000,0x0076,0,65535,32.1,8414,259,265,223,150,175,86,2377,2779,65535,98,0,65535,-2000,71,2000,8700,0x0080,3,96,0x0186,0x1000,0x10,0x0008,0x10,0x0814,0x0038,0x0000,0x0000,0x0000,0x0000,0x0000,0x0000,0x0000,0x0000,4209,4207,8417,8420,257,257,108,108,218,32.1,-53.5,32.1,2377,1791,2779,2129,0,2377,1791,423,355,2779,2129,27.6,27.4,1000,1000,0,0,0,14,0,0,236,2448,2432,-21,-17,1,0,0,2858,2849,0,0,-21,1,3.76,3413,2448,2432,0,1820,2448,2432,16384,953,SUCCESS
    61,2022-10-28 05:38:54,244.000,0x0076,0,65535,32.2,8414,258,263,221,150,175,86,2377,2779,65535,98,0,65535,-2000,71,2000,8700,0x0080,3,96,0x0186,0x1000,0x10,0x0008,0x10,0x0814,0x0038,0x0000,0x0000,0x0000,0x0000,0x0000,0x0000,0x0000,0x0000,4208,4207,8416,8421,256,257,108,108,217,32.1,-53.5,32.1,2377,1791,2779,2129,0,2377,1791,423,355,2779,2129,27.6,27.4,1000,1000,0,0,0,14,0,0,240,2448,2432,-21,-17,1,0,0,2858,2849,0,0,-22,1,3.76,3413,2448,2432,0,1816,2448,2432,16384,953,SUCCESS
    62,2022-10-28 05:38:58,248.000,0x0076,0,65535,32.1,8415,256,261,220,150,175,86,2378,2779,65535,98,0,65535,-2000,71,2000,8700,0x0080,3,96,0x0186,0x1000,0x10,0x0008,0x10,0x0814,0x0038,0x0000,0x0000,0x0000,0x0000,0x0000,0x0000,0x0000,0x0000,4208,4206,8418,8422,255,254,107,107,215,32.1,-53.4,32.1,2378,1792,2779,2129,0,2378,1792,423,355,2779,2129,27.6,27.4,1000,1000,0,0,0,14,0,0,244,2448,2432,-22,-18,1,0,0,2858,2849,0,0,-22,1,3.76,3413,2448,2432,0,1812,2448,2432,16384,969,SUCCESS
    63,2022-10-28 05:39:02,252.000,0x0076,0,65535,32.1,8415,255,260,219,150,175,86,2378,2779,65535,99,0,65535,-2000,71,2000,8700,0x0080,3,96,0x0186,0x1000,0x10,0x0008,0x10,0x0814,0x0038,0x0000,0x0000,0x0000,0x0000,0x0000,0x0000,0x0000,0x0000,4209,4207,8418,8420,254,252,107,106,215,32.1,-53.4,32.1,2378,1792,2779,2129,0,2378,1792,423,355,2779,2129,27.6,27.4,1000,1000,0,0,0,14,0,0,248,2448,2432,-22,-18,1,0,0,2858,2849,0,0,-22,1,3.76,3413,2448,2432,0,1808,2448,2432,16384,953,SUCCESS
    64,2022-10-28 05:39:06,256.000,0x0076,0,65535,32.1,8416,254,258,218,150,175,86,2378,2779,65535,100,0,65535,-2000,71,2000,8700,0x0080,3,96,0x0186,0x1000,0x10,0x0008,0x10,0x0814,0x0038,0x0000,0x0000,0x0000,0x0000,0x0000,0x0000,0x0000,0x0000,4209,4207,8417,8421,252,250,106,105,214,32.2,-53.4,32.1,2378,1792,2779,2129,0,2378,1792,423,355,2779,2129,27.6,27.4,1000,1000,0,0,0,14,0,0,252,2448,2432,-22,-18,1,0,0,2858,2849,0,0,-22,1,3.76,3413,2448,2432,0,1804,2448,2432,16384,969,SUCCESS
    65,2022-10-28 05:39:10,260.000,0x0076,0,65535,32.1,8416,252,257,216,150,175,86,2379,2779,65535,99,0,65535,-2000,71,2000,8700,0x0080,3,96,0x0186,0x1000,0x10,0x0008,0x10,0x0814,0x0038,0x0000,0x0000,0x0000,0x0000,0x0000,0x0000,0x0000,0x0000,4209,4207,8418,8421,250,249,105,105,212,32.1,-53.4,32.1,2379,1793,2779,2129,0,2379,1793,423,355,2779,2129,27.6,27.4,1000,1000,0,0,0,14,0,0,256,2448,2432,-23,-19,1,0,0,2858,2849,0,0,-23,1,3.76,3413,2448,2432,0,1800,2448,2432,16384,969,SUCCESS
    66,2022-10-28 05:39:14,264.000,0x0076,0,65535,32.1,8416,251,256,215,150,175,86,2379,2779,65535,100,0,65535,-2000,71,2000,8700,0x0080,3,96,0x0186,0x1000,0x10,0x0008,0x10,0x0814,0x0038,0x0000,0x0000,0x0000,0x0000,0x0000,0x0000,0x0000,0x0000,4209,4207,8417,8422,247,248,104,104,211,32.1,-53.4,32.1,2379,1793,2779,2129,0,2379,1793,423,355,2779,2129,27.6,27.4,1000,1000,0,0,0,14,0,0,260,2448,2432,-23,-19,1,0,0,2858,2849,0,0,-23,1,3.76,3413,2448,2432,0,1796,2448,2432,16384,953,SUCCESS
    67,2022-10-28 05:39:18,268.000,0x0076,0,65535,32.0,8416,250,254,214,150,175,86,2379,2779,65535,101,0,65535,-2000,71,2000,8700,0x0080,3,96,0x0186,0x1000,0x10,0x0008,0x10,0x0814,0x0038,0x0000,0x0000,0x0000,0x0000,0x0000,0x0000,0x0000,0x0000,4209,4207,8418,8421,247,246,104,103,210,32.1,-53.5,32.0,2379,1793,2779,2129,0,2379,1793,423,355,2779,2129,27.6,27.4,1000,1000,0,0,0,14,0,0,264,2448,2432,-23,-19,1,0,0,2858,2849,0,0,-23,1,3.76,3413,2448,2432,0,1792,2448,2432,16384,953,SUCCESS
    68,2022-10-28 05:39:22,272.000,0x0076,0,65535,32.1,8415,248,253,213,150,175,86,2379,2779,65535,101,0,65535,-2000,71,2000,8700,0x0080,3,96,0x0186,0x1000,0x10,0x0008,0x10,0x0814,0x0038,0x0000,0x0000,0x0000,0x0000,0x0000,0x0000,0x0000,0x0000,4209,4207,8416,8420,247,247,104,104,208,32.1,-53.5,32.1,2379,1793,2779,2129,0,2379,1793,423,355,2779,2129,27.6,27.4,1000,1000,0,0,0,14,0,0,268,2448,2432,-23,-19,1,0,0,2858,2849,0,0,-23,1,3.76,3413,2448,2432,0,1788,2448,2432,16384,953,SUCCESS
    69,2022-10-28 05:39:26,276.000,0x0076,0,65535,32.1,8416,247,251,212,150,175,86,2380,2779,65535,101,0,65535,-2000,71,2000,8700,0x0080,3,96,0x0186,0x1000,0x10,0x0008,0x10,0x0814,0x0038,0x0000,0x0000,0x0000,0x0000,0x0000,0x0000,0x0000,0x0000,4209,4207,8416,8423,246,243,104,102,207,32.1,-53.4,32.1,2380,1794,2779,2129,0,2380,1794,423,355,2779,2129,27.6,27.4,1000,1000,0,0,0,14,0,0,272,2448,2432,-24,-20,1,0,0,2858,2849,0,0,-24,1,3.76,3413,2448,2432,0,1784,2448,2432,16384,969,SUCCESS
    70,2022-10-28 05:39:30,280.000,0x0076,0,65535,32.1,8416,246,250,211,150,175,86,2380,2779,65535,102,0,65535,-2000,71,2000,8700,0x0080,3,96,0x0186,0x1000,0x10,0x0008,0x10,0x0814,0x0038,0x0000,0x0000,0x0000,0x0000,0x0000,0x0000,0x0000,0x0000,4209,4207,8417,8420,245,244,103,103,206,32.1,-53.3,32.1,2380,1794,2779,2129,0,2380,1794,423,355,2779,2129,27.6,27.4,1000,1000,0,0,0,14,0,0,276,2448,2432,-24,-20,1,0,0,2858,2849,0,0,-24,1,3.76,3413,2448,2432,0,1780,2448,2432,16384,969,SUCCESS
    71,2022-10-28 05:39:34,284.000,0x0076,0,65535,32.0,8415,244,249,209,150,175,86,2380,2779,65535,102,0,65535,-2000,71,2000,8700,0x0080,3,96,0x0186,0x1000,0x10,0x0008,0x10,0x0814,0x0038,0x0000,0x0000,0x0000,0x0000,0x0000,0x0000,0x0000,0x0000,4209,4207,8417,8420,241,242,101,102,205,32.1,-53.4,32.0,2380,1794,2779,2129,0,2380,1794,423,355,2779,2129,27.6,27.4,1000,1000,0,0,0,14,0,0,280,2448,2432,-24,-20,1,0,0,2858,2849,0,0,-24,1,3.76,3413,2448,2432,0,1776,2448,2432,16384,969,SUCCESS
    72,2022-10-28 05:39:38,288.000,0x0076,0,65535,32.0,8416,243,247,208,150,175,86,2380,2779,65535,103,0,65535,-2000,71,2000,8700,0x0080,3,96,0x0186,0x1000,0x10,0x0008,0x10,0x0814,0x0038,0x0000,0x0000,0x0000,0x0000,0x0000,0x0000,0x0000,0x0000,4210,4207,8418,8422,245,243,103,102,207,32.0,-53.5,32.0,2380,1794,2779,2129,0,2381,1794,423,355,2779,2129,27.6,27.4,1000,1000,0,0,0,14,0,0,284,2448,2432,-25,-20,1,0,0,2858,2849,0,0,-25,1,3.76,3413,2448,2432,0,1772,2448,2432,16384,953,SUCCESS
    73,2022-10-28 05:39:42,292.000,0x0076,0,65535,32.0,8420,265,247,208,150,175,86,2381,2779,65535,103,0,65535,-2000,71,2000,8700,0x0080,3,96,0x0186,0x1000,0x10,0x0008,0x10,0x0814,0x0038,0x0000,0x0000,0x0000,0x0000,0x0000,0x0000,0x0000,0x0000,4212,4210,8421,8426,276,277,116,117,228,32.0,-53.3,32.0,2381,1794,2779,2129,0,2381,1794,423,355,2779,2129,27.6,27.4,1000,1000,0,0,0,14,0,0,288,2448,2432,-25,-20,1,0,0,2858,2849,0,0,-25,1,3.76,3413,2448,2432,0,1767,2448,2432,16384,969,SUCCESS
    74,2022-10-28 05:39:46,296.000,0x0076,0,65535,32.0,8434,339,265,224,150,175,86,2381,2779,65535,96,0,65535,-2000,71,2000,8700,0x0080,3,96,0x0186,0x1000,0x10,0x0008,0x10,0x0814,0x0038,0x0000,0x0000,0x0000,0x0000,0x0000,0x0000,0x0000,0x0000,4218,4216,8435,8440,338,337,143,142,285,32.0,-53.5,32.0,2381,1794,2779,2129,0,2381,1794,423,355,2779,2129,27.6,27.4,1000,1000,0,0,0,14,0,0,292,2448,2432,-25,-20,1,0,0,2858,2849,0,0,-25,1,3.76,3413,2448,2432,0,1763,2448,2432,16384,953,SUCCESS
    75,2022-10-28 05:39:50,300.000,0x0076,0,65535,32.0,8434,335,282,238,150,175,86,2381,2779,65535,91,0,65535,-2000,71,2000,8700,0x0080,3,96,0x0186,0x1000,0x10,0x0008,0x10,0x0814,0x0038,0x0000,0x0000,0x0000,0x0000,0x0000,0x0000,0x0000,0x0000,4219,4216,8436,8441,333,333,140,140,283,32.0,-53.4,32.0,2382,1795,2779,2129,0,2382,1795,423,355,2779,2129,27.6,27.4,1000,1000,0,0,0,14,0,0,296,2448,2432,-26,-21,1,0,0,2858,2849,0,0,-26,1,3.76,3413,2448,2432,0,1759,2448,2432,16384,969,SUCCESS
    76,2022-10-28 05:39:54,304.000,0x0076,0,65535,32.0,8435,335,295,249,150,175,86,2382,2779,65535,88,0,65535,-2000,71,2000,8700,0x0080,3,96,0x0186,0x1000,0x10,0x0008,0x10,0x0814,0x0038,0x0000,0x0000,0x0000,0x0000,0x0000,0x0000,0x0000,0x0000,4219,4216,8436,8442,332,331,140,140,283,32.0,-53.3,32.0,2382,1795,2779,2129,0,2382,1795,423,355,2779,2129,27.6,27.4,1000,1000,0,0,0,14,0,0,300,2448,2432,-26,-21,1,0,0,2858,2849,0,0,-26,1,3.76,3413,2448,2432,0,1755,2448,2432,16384,969,SUCCESS
    77,2022-10-28 05:39:58,308.000,0x0076,0,65535,32.0,8435,333,304,257,150,175,86,2382,2779,65535,94,0,65535,-2000,71,2000,8700,0x0080,3,96,0x0186,0x1000,0x10,0x0008,0x10,0x0814,0x0038,0x0000,0x0000,0x0000,0x0000,0x0000,0x0000,0x0000,0x0000,4219,4217,8436,8444,329,328,139,138,280,32.0,-53.4,32.0,2382,1795,2779,2129,0,2382,1795,423,355,2779,2129,27.6,27.4,1000,1000,0,0,0,14,0,0,304,2448,2432,-26,-21,1,0,0,2858,2849,0,0,-26,1,3.76,3413,2448,2432,0,1751,2448,2432,16384,953,SUCCESS
    78,2022-10-28 05:40:02,312.000,0x0076,0,65535,32.0,8436,326,310,262,150,175,86,2383,2779,65535,92,0,65535,-2000,71,2000,8700,0x0080,3,96,0x0186,0x1000,0x10,0x0008,0x10,0x0814,0x0038,0x0000,0x0000,0x0000,0x0000,0x0000,0x0000,0x0000,0x0000,4218,4215,8438,8441,285,282,120,119,265,32.0,-53.5,32.0,2383,1796,2779,2129,0,2383,1796,423,355,2779,2129,27.6,27.4,1000,1000,0,0,0,14,0,0,309,2448,2432,-27,-22,1,0,0,2858,2849,0,0,-27,1,3.76,3413,2448,2432,0,1747,2448,2432,16384,953,SUCCESS
    79,2022-10-28 05:40:06,316.000,0x0076,0,65535,32.1,8445,376,320,270,150,175,86,2383,2779,65535,90,0,65535,-2000,71,2000,8700,0x0080,3,96,0x0186,0x1000,0x10,0x0008,0x10,0x0814,0x0038,0x0000,0x0000,0x0000,0x0000,0x0000,0x0000,0x0000,0x0000,4224,4222,8445,8452,378,378,160,160,321,32.0,-53.5,32.0,2383,1796,2779,2129,0,2383,1796,423,355,2779,2129,27.6,27.4,1000,1000,0,0,0,14,0,0,313,2448,2432,-27,-22,1,0,0,2858,2849,0,0,-27,1,3.76,3413,2448,2432,0,1743,2448,2432,16384,953,SUCCESS
    80,2022-10-28 05:40:10,320.000,0x0076,0,65535,32.1,8448,382,335,283,150,175,86,2383,2779,65535,87,0,65535,-2000,71,2000,8700,0x0080,3,96,0x0186,0x1000,0x10,0x0008,0x10,0x0814,0x0038,0x0000,0x0000,0x0000,0x0000,0x0000,0x0000,0x0000,0x0000,4225,4223,8447,8456,383,379,162,160,323,32.0,-53.5,32.1,2383,1797,2779,2129,0,2384,1797,423,355,2779,2129,27.6,27.4,1000,1000,0,0,0,14,0,0,317,2448,2432,-28,-23,1,0,0,2858,2849,0,0,-28,1,3.76,3413,2448,2432,0,1739,2448,2432,16384,953,SUCCESS
    81,2022-10-28 05:40:14,324.000,0x0076,0,65535,32.1,8447,373,345,292,150,175,86,2384,2779,65535,86,0,65535,-2000,72,2000,8700,0x0080,3,96,0x0186,0x1000,0x10,0x0008,0x10,0x0814,0x0038,0x0000,0x0000,0x0000,0x0000,0x0000,0x0000,0x0000,0x0000,4225,4222,8447,8454,368,369,155,156,313,32.0,-53.4,32.1,2384,1797,2779,2129,0,2384,1797,423,355,2779,2129,27.6,27.4,1000,1000,0,0,0,14,0,0,321,2448,2432,-28,-23,1,0,0,2858,2849,0,0,-28,1,3.76,3413,2448,2432,0,1735,2448,2432,16384,953,SUCCESS
    82,2022-10-28 05:40:18,328.000,0x0076,0,65535,32.1,8450,383,353,298,150,175,86,2384,2779,65535,84,0,65535,-2000,72,2000,8700,0x0080,3,96,0x0186,0x1000,0x10,0x0008,0x10,0x0814,0x0038,0x0000,0x0000,0x0000,0x0000,0x0000,0x0000,0x0000,0x0000,4226,4224,8450,8457,381,379,161,160,324,32.0,-53.3,32.1,2384,1797,2779,2129,0,2384,1797,423,355,2779,2129,27.6,27.4,1000,1000,0,0,0,14,0,0,325,2448,2432,-28,-23,1,0,0,2858,2849,0,0,-28,1,3.76,3413,2448,2432,0,1731,2448,2432,16384,953,SUCCESS
    83,2022-10-28 05:40:22,332.000,0x0076,0,65535,32.1,8450,375,361,305,150,175,86,2385,2779,65535,83,0,65535,-2000,72,2000,8700,0x0080,3,96,0x0186,0x1000,0x10,0x0008,0x10,0x0814,0x0038,0x0000,0x0000,0x0000,0x0000,0x0000,0x0000,0x0000,0x0000,4226,4223,8450,8456,370,367,156,155,313,32.0,-53.4,32.1,2385,1798,2779,2129,0,2385,1798,423,355,2779,2129,27.6,27.4,1000,1000,0,0,0,14,0,0,329,2448,2432,-29,-24,1,0,0,2858,2849,0,0,-29,1,3.76,3413,2448,2432,0,1727,2448,2432,16384,953,SUCCESS
    84,2022-10-28 05:40:26,336.000,0x0076,0,65535,32.1,8450,373,365,308,150,175,86,2385,2779,65535,82,0,65535,-2000,72,2000,8700,0x0080,3,96,0x0186,0x1000,0x10,0x0008,0x10,0x0814,0x0038,0x0000,0x0000,0x0000,0x0000,0x0000,0x0000,0x0000,0x0000,4226,4223,8451,8457,365,362,154,153,315,32.0,-53.4,32.1,2385,1798,2779,2129,0,2385,1798,423,355,2779,2129,27.6,27.4,1000,1000,0,0,0,14,0,0,333,2448,2432,-29,-24,1,0,0,2858,2849,0,0,-29,1,3.76,3413,2448,2432,0,1723,2448,2432,16384,953,SUCCESS
    85,2022-10-28 05:40:30,340.000,0x0076,0,65535,32.1,8466,461,376,318,150,175,86,2386,2779,65535,81,0,65535,-2000,72,2000,8700,0x0080,3,96,0x0186,0x1000,0x10,0x0008,0x10,0x0814,0x0038,0x0000,0x0000,0x0000,0x0000,0x0000,0x0000,0x0000,0x0000,4234,4231,8466,8474,452,453,191,192,387,32.1,-53.5,32.1,2386,1799,2779,2129,0,2386,1799,423,355,2779,2129,27.6,27.4,1000,1000,0,0,0,14,0,0,337,2448,2432,-30,-25,1,0,0,2858,2849,0,0,-30,1,3.76,3413,2448,2432,0,1719,2448,2432,16384,953,SUCCESS
    86,2022-10-28 05:40:34,344.000,0x0076,0,65535,32.1,8465,441,393,332,150,175,86,2386,2779,65535,78,0,65535,-2000,72,2000,8700,0x0080,3,96,0x0186,0x1000,0x10,0x0008,0x10,0x0814,0x0038,0x0000,0x0000,0x0000,0x0000,0x0000,0x0000,0x0000,0x0000,4233,4231,8465,8473,438,438,185,185,373,32.1,-53.5,32.1,2386,1799,2779,2129,0,2386,1799,423,355,2779,2129,27.6,27.4,1000,1000,0,0,0,14,0,0,341,2448,2432,-30,-25,1,0,0,2858,2849,0,0,-30,1,3.76,3413,2448,2432,0,1715,2448,2432,16384,953,SUCCESS
    87,2022-10-28 05:40:38,348.000,0x0076,0,65535,32.1,8469,460,405,342,150,175,86,2386,2779,65535,77,0,65535,-2000,72,2000,8700,0x0080,3,96,0x0186,0x1000,0x10,0x0008,0x10,0x0814,0x0038,0x0000,0x0000,0x0000,0x0000,0x0000,0x0000,0x0000,0x0000,4240,4237,8475,8478,550,550,233,233,442,32.1,-53.5,32.1,2387,1800,2779,2129,0,2387,1800,423,355,2779,2129,27.6,27.4,1000,1000,0,0,0,14,0,0,345,2448,2432,-31,-26,1,0,0,2858,2849,0,0,-31,1,3.76,3413,2448,2432,0,1711,2448,2432,16384,953,SUCCESS
    88,2022-10-28 05:40:42,352.000,0x0076,0,65535,32.1,8530,844,466,395,150,175,86,2387,2779,65535,76,0,65535,-2000,72,2000,8700,0x4080,3,96,0x0186,0x1000,0x10,0x0008,0x10,0x0814,0x0038,0x0002,0x0000,0x0000,0x0000,0x0000,0x0000,0x0000,0x0000,4268,4264,8530,8549,834,838,356,357,708,32.2,-53.5,32.2,2387,1800,2779,2129,0,2388,1800,423,355,2779,2129,27.6,27.4,1000,1000,0,0,0,14,0,0,349,2448,2432,-32,-26,1,0,0,2858,2849,0,0,-32,1,3.76,3413,2448,2432,0,1707,2448,2432,16384,953,SUCCESS
    89,2022-10-28 05:40:46,356.000,0x0076,0,65535,32.2,8394,0,399,338,150,175,86,2387,2779,65535,77,0,65535,-2000,72,0,0,0x0080,3,96,0x4982,0x1000,0x10,0x0008,0x10,0x0814,0x0038,0x0000,0x0002,0x0000,0x0000,0x0000,0x0000,0x0000,0x0000,4197,4195,8393,8604,0,0,0,0,0,32.2,-53.4,32.2,2387,1800,2779,2129,0,2388,1800,423,355,2779,2129,27.6,27.4,1000,1000,0,0,0,14,0,0,353,2448,2432,-32,-26,1,0,0,2858,2849,0,0,-32,1,3.76,3413,2448,2432,0,1703,2448,2432,16384,953,SUCCESS
    90,2022-10-28 05:40:50,360.000,0x0076,0,65535,32.2,8389,0,303,257,150,175,86,2387,2779,65535,92,0,65535,-2000,72,0,0,0x0080,3,96,0x4982,0x1000,0x10,0x0008,0x10,0x0814,0x0038,0x0000,0x0002,0x0000,0x0000,0x0000,0x0000,0x0000,0x0000,4195,4193,8390,8605,0,0,0,0,0,32.1,-53.4,32.1,2387,1800,2779,2129,0,2388,1800,423,355,2779,2129,27.6,27.4,1000,1000,0,0,0,14,0,0,357,2448,2432,-32,-26,1,0,0,2858,2849,0,0,-32,1,3.76,3413,2448,2432,0,1699,2448,2432,16384,953,SUCCESS
    91,2022-10-28 05:40:54,364.000,0x0076,0,65535,32.1,8387,0,230,195,150,175,86,2387,2779,65535,107,0,65535,-2000,72,0,0,0x0080,3,96,0x4982,0x1000,0x10,0x0008,0x10,0x0814,0x0038,0x0000,0x0002,0x0000,0x0000,0x0000,0x0000,0x0000,0x0000,4193,4192,8387,8324,0,0,0,0,0,32.1,-53.5,32.1,2387,1800,2779,2129,0,2388,1800,423,355,2779,2129,27.6,27.4,1000,1000,0,0,0,14,0,0,361,2448,2432,-32,-26,1,0,0,2858,2849,0,0,-32,1,3.76,3413,2448,2432,0,1695,2448,2432,16384,953,SUCCESS
    92,2022-10-28 05:40:58,368.000,0x0076,0,65535,32.2,8384,0,175,148,150,175,86,2387,2779,65535,136,0,65535,-2000,72,0,0,0x0080,3,96,0x4982,0x1000,0x10,0x0008,0x10,0x0814,0x0038,0x0000,0x0002,0x0000,0x0000,0x0000,0x0000,0x0000,0x0000,4192,4191,8383,8324,0,0,0,0,0,32.1,-53.4,32.1,2387,1800,2779,2129,0,2388,1800,423,355,2779,2129,27.6,27.4,1000,1000,0,0,0,14,0,0,365,2448,2432,-32,-26,1,0,0,2858,2849,0,0,-32,1,3.76,3413,2448,2432,0,1691,2448,2432,16384,969,SUCCESS
    93,2022-10-28 05:41:02,372.000,0x0076,0,65535,32.2,8381,0,133,113,150,175,86,2387,2779,65535,176,0,65535,-2000,72,0,0,0x0080,3,96,0x4982,0x1000,0x10,0x0008,0x10,0x0814,0x0038,0x0000,0x0002,0x0000,0x0000,0x0000,0x0000,0x0000,0x0000,4192,4190,8385,8318,0,0,0,0,0,32.2,-53.5,32.1,2387,1800,2779,2129,0,2388,1800,423,355,2779,2129,27.6,27.4,1000,1000,0,0,0,14,0,0,369,2448,2432,-32,-26,1,0,0,2858,2849,0,0,-32,1,3.76,3413,2448,2432,0,1687,2448,2432,16384,953,SUCCESS
    94,2022-10-28 05:41:06,376.000,0x0076,0,65535,32.1,8381,0,101,86,150,175,86,2387,2779,65535,232,0,65535,-2000,72,0,0,0x0080,3,96,0x4982,0x1000,0x10,0x0008,0x10,0x0814,0x0038,0x0000,0x0002,0x0000,0x0000,0x0000,0x0000,0x0000,0x0000,4191,4190,8384,8315,0,0,0,0,0,32.2,-53.4,32.1,2387,1800,2779,2129,0,2388,1800,423,355,2779,2129,27.6,27.4,1000,1000,0,0,0,14,0,0,373,2448,2432,-32,-26,1,0,0,2858,2849,0,0,-32,1,3.76,3413,2448,2432,0,1683,2448,2432,16384,953,SUCCESS
    95,2022-10-28 05:41:10,380.000,0x0076,0,65535,32.1,8380,0,77,65,150,175,86,2387,2779,65535,305,0,65535,-2000,72,0,0,0x0080,3,96,0x4982,0x1000,0x10,0x0008,0x10,0x0814,0x0038,0x0000,0x0002,0x0000,0x0000,0x0000,0x0000,0x0000,0x0000,4190,4189,8380,8314,0,0,0,0,0,32.1,-53.4,32.1,2387,1800,2779,2129,0,2388,1800,423,355,2779,2129,27.6,27.4,1000,1000,0,0,0,14,0,0,377,2448,2432,-32,-26,1,0,0,2858,2849,0,0,-32,1,3.76,3413,2448,2432,0,1679,2448,2432,16384,953,SUCCESS
    96,2022-10-28 05:41:14,384.000,0x0076,0,65535,32.0,8378,0,58,49,150,175,86,2387,2779,65535,404,0,65535,-2000,72,0,0,0x0080,3,96,0x4982,0x1000,0x10,0x0008,0x10,0x0814,0x0038,0x0000,0x0002,0x0000,0x0000,0x0000,0x0000,0x0000,0x0000,4190,4189,8381,8314,0,0,0,0,0,32.0,-53.4,32.0,2387,1800,2779,2129,0,2388,1800,423,355,2779,2129,27.6,27.4,1000,1000,0,0,0,14,0,0,381,2448,2432,-32,-26,1,0,0,2858,2849,0,0,-32,1,3.76,3413,2448,2432,0,1675,2448,2432,16384,969,SUCCESS
    97,2022-10-28 05:41:18,388.000,0x0076,0,65535,32.0,8378,0,44,38,150,175,86,2387,2779,65535,533,0,65535,-2000,72,0,0,0x0080,3,96,0x4982,0x1000,0x10,0x0008,0x10,0x0814,0x0038,0x0000,0x0002,0x0000,0x0000,0x0000,0x0000,0x0000,0x0000,4189,4188,8379,8317,0,0,0,0,0,32.0,-53.4,32.0,2387,1800,2779,2129,0,2388,1800,423,355,2779,2129,27.6,27.4,1000,1000,0,0,0,14,0,0,385,2448,2432,-32,-26,2,0,0,2858,2849,0,0,-32,2,3.76,3413,2448,2432,0,1671,2448,2432,16384,969,SUCCESS
    98,2022-10-28 05:41:22,392.000,0x0076,0,65535,32.0,8377,0,34,29,150,175,86,2387,2779,65535,690,0,65535,-2000,72,0,0,0x0080,3,96,0x4982,0x1000,0x10,0x0008,0x10,0x0814,0x0038,0x0000,0x0002,0x0000,0x0000,0x0000,0x0000,0x0000,0x0000,4189,4188,8378,8311,0,0,0,0,0,32.1,-53.3,32.0,2387,1800,2779,2129,0,2388,1800,423,355,2779,2129,27.6,27.4,1000,1000,0,0,0,14,0,0,389,2448,2432,-32,-26,2,0,0,2858,2849,0,0,-32,2,3.76,3413,2448,2432,0,1667,2448,2432,16384,969,SUCCESS
    99,2022-10-28 05:41:26,396.000,0x0076,0,65535,32.0,8376,0,26,22,150,175,86,2387,2779,65535,902,0,65535,-2000,72,0,0,0x0080,3,96,0x4982,0x1000,0x10,0x0008,0x10,0x0814,0x0038,0x0000,0x0002,0x0000,0x0000,0x0000,0x0000,0x0000,0x0000,4189,4188,8379,8311,0,0,0,0,0,32.0,-53.5,32.0,2387,1800,2779,2129,0,2388,1800,423,355,2779,2129,27.6,27.4,1000,1000,0,0,0,14,0,0,393,2448,2432,-32,-26,2,0,0,2858,2849,0,0,-32,2,3.76,3413,2448,2432,0,1663,2448,2432,16384,969,SUCCESS
    100,2022-10-28 05:41:30,400.000,0x0076,0,65535,31.9,8376,0,19,16,150,175,86,2387,2779,65535,1235,0,65535,-2000,72,0,0,0x0080,3,96,0x4982,0x1000,0x10,0x0008,0x10,0x0814,0x0038,0x0000,0x0002,0x0000,0x0000,0x0000,0x0000,0x0000,0x0000,4189,4187,8378,8310,0,0,0,0,0,32.0,-53.4,32.0,2387,1800,2779,2129,0,2388,1800,423,355,2779,2129,27.6,27.4,1000,1000,0,0,0,14,0,0,397,2448,2432,-32,-26,2,0,0,2858,2849,0,0,-32,2,3.76,3413,2448,2432,0,1659,2448,2432,16384,969,SUCCESS
    101,2022-10-28 05:41:34,404.000,0x0076,0,65535,31.9,8375,0,15,12,150,175,86,2387,2779,65535,1564,0,65535,-2000,72,0,0,0x0080,3,96,0x4982,0x1000,0x10,0x0008,0x10,0x0814,0x0038,0x0000,0x0002,0x0000,0x0000,0x0000,0x0000,0x0000,0x0000,4189,4187,8376,8307,0,0,0,0,0,31.9,-53.4,31.9,2387,1800,2779,2129,0,2388,1800,423,355,2779,2129,27.6,27.4,1000,1000,0,0,0,14,0,0,401,2448,2432,-32,-26,2,0,0,2858,2849,0,0,-32,2,3.76,3413,2448,2432,0,1655,2448,2432,16384,953,SUCCESS
    102,2022-10-28 05:41:38,408.000,0x0076,0,65535,31.9,8375,0,11,9,150,175,86,2387,2779,65535,2133,0,65535,-2000,72,0,0,0x0080,3,96,0x4982,0x1000,0x10,0x0008,0x10,0x0814,0x0038,0x0000,0x0002,0x0000,0x0000,0x0000,0x0000,0x0000,0x0000,4188,4187,8376,8311,0,0,0,0,0,31.9,-53.4,31.9,2387,1800,2779,2129,0,2388,1800,423,355,2779,2129,27.6,27.4,1000,1000,0,0,0,14,0,0,405,2448,2432,-32,-26,2,0,0,2858,2849,0,0,-32,2,3.76,3413,2448,2432,0,1651,2448,2432,16384,969,SUCCESS
    103,2022-10-28 05:41:42,412.000,0x0076,0,65535,31.9,8374,0,8,7,150,175,86,2387,2779,65535,2933,0,65535,-2000,72,0,0,0x0080,3,96,0x4982,0x1000,0x10,0x0008,0x10,0x0814,0x0038,0x0000,0x0002,0x0000,0x0000,0x0000,0x0000,0x0000,0x0000,4188,4187,8376,8312,0,0,0,0,0,31.9,-53.4,31.9,2387,1800,2779,2129,0,2388,1800,423,355,2779,2129,27.6,27.4,1000,1000,0,0,0,14,0,0,409,2448,2432,-32,-26,2,0,0,2858,2849,0,0,-32,2,3.76,3413,2448,2432,0,1647,2448,2432,16384,969,SUCCESS
    104,2022-10-28 05:41:46,416.000,0x0076,0,65535,30.1,8374,0,0,0,150,175,86,2387,2779,65535,65535,0,65535,-2000,72,0,0,0x00C0,3,96,0x4982,0x0000,0x10,0x0008,0x50,0x0814,0x0038,0x0000,0x0002,0x0000,0x0000,0x0000,0x0000,0x0000,0x0000,4187,4187,8376,8373,0,0,0,0,0,29.9,-53.4,29.9,2387,1800,2779,2129,0,2388,1800,423,355,2779,2129,27.6,27.4,1000,1000,0,0,0,14,0,0,4,2448,2432,-32,-26,2,0,0,2858,2849,0,0,-32,2,3.76,3413,2448,2432,0,1647,2448,2432,16384,969,SUCCESS
    105,2022-10-28 05:41:50,420.000,0x0076,0,65535,29.6,8374,0,0,0,150,175,86,2387,2779,65535,65535,0,65535,-2000,72,0,0,0x00C0,3,96,0x4982,0x0000,0x10,0x0008,0x50,0x0814,0x0038,0x0000,0x0002,0x0000,0x0000,0x0000,0x0000,0x0000,0x0000,4187,4187,8376,8077,0,0,0,0,0,29.5,-53.3,29.5,2387,1800,2779,2129,0,2388,1800,423,355,2779,2129,27.6,27.4,1000,1000,0,0,0,14,0,0,8,2448,2432,-32,-26,2,0,0,2858,2849,0,0,-32,2,3.76,3413,2448,2432,0,1647,2448,2432,16384,969,SUCCESS
    106,2022-10-28 05:41:54,424.000,0x0076,0,65535,29.2,8374,0,0,0,150,175,86,2387,2779,65535,65535,0,65535,-2000,72,0,0,0x00C0,3,96,0x4982,0x0000,0x10,0x0008,0x50,0x0814,0x0038,0x0000,0x0002,0x0000,0x0000,0x0000,0x0000,0x0000,0x0000,4187,4186,8374,8077,0,0,0,0,0,29.2,-53.3,29.2,2387,1800,2779,2129,0,2388,1800,423,355,2779,2129,27.6,27.4,1000,1000,0,0,0,14,0,0,12,2448,2432,-32,-26,2,0,0,2858,2849,0,0,-32,2,3.76,3413,2448,2432,0,1647,2448,2432,16384,969,SUCCESS
    107,2022-10-28 05:41:58,428.000,0x0076,0,65535,29.0,8373,0,0,0,150,175,86,2387,2779,65535,65535,0,65535,-2000,72,0,0,0x00C0,3,96,0x4982,0x0000,0x10,0x0008,0x50,0x0814,0x0038,0x0000,0x0002,0x0000,0x0000,0x0000,0x0000,0x0000,0x0000,4186,4187,8376,8077,0,0,0,0,0,29.0,-53.5,29.0,2387,1800,2779,2129,0,2388,1800,423,355,2779,2129,27.6,27.4,1000,1000,0,0,0,14,0,0,16,2448,2432,-32,-26,2,0,0,2858,2849,0,0,-32,2,3.76,3413,2448,2432,0,1647,2448,2432,16384,953,SUCCESS
    108,2022-10-28 05:42:02,432.000,0x0076,0,65535,28.8,8372,0,0,0,150,175,86,2387,2779,65535,65535,0,65535,-2000,72,0,0,0x00C0,3,96,0x4982,0x0000,0x08,0x0008,0x50,0x0814,0x0038,0x0000,0x0002,0x0000,0x0000,0x0000,0x0000,0x0000,0x0000,4186,4186,8375,8372,0,0,0,0,0,28.8,-53.5,28.8,2387,1800,2779,2129,0,2388,1800,423,355,2779,2129,27.6,27.4,1000,1000,0,0,0,14,0,0,20,2448,2432,-32,-26,2,0,0,2858,2849,0,0,-32,2,3.76,3413,2448,2432,0,1647,2448,2432,16384,969,SUCCESS
    109,2022-10-28 05:42:06,436.000,0x0076,0,65535,28.7,8372,0,0,0,150,175,86,2387,2779,65535,65535,0,65535,-2000,72,0,0,0x00C0,3,96,0x4982,0x0000,0x08,0x0008,0x50,0x0814,0x0038,0x0000,0x0002,0x0000,0x0000,0x0000,0x0000,0x0000,0x0000,4186,4186,8373,8375,0,0,0,0,0,28.6,-53.3,28.6,2387,1800,2779,2129,0,2388,1800,423,355,2779,2129,27.6,27.4,1000,1000,0,0,0,14,0,0,24,2448,2432,-32,-26,2,0,0,2858,2849,0,0,-32,2,3.76,3413,2448,2432,0,1647,2448,2432,16384,969,SUCCESS
    110,2022-10-28 05:42:10,440.000,0x0076,0,65535,28.5,8372,0,0,0,150,175,86,2387,2779,65535,65535,0,65535,-2000,72,0,0,0x00C0,3,96,0x4982,0x0000,0x08,0x0008,0x50,0x0814,0x0038,0x0000,0x0002,0x0000,0x0000,0x0000,0x0000,0x0000,0x0000,4186,4186,8374,8374,0,0,0,0,0,28.5,-53.4,28.5,2387,1800,2779,2129,0,2388,1800,423,355,2779,2129,27.6,27.4,1000,1000,0,0,0,14,0,0,28,2448,2432,-32,-26,2,0,0,2858,2849,0,0,-32,2,3.76,3413,2448,2432,0,1647,2448,2432,16384,953,SUCCESS
    111,2022-10-28 05:42:14,444.000,0x0076,0,65535,28.4,8371,0,0,0,150,175,86,2387,2779,65535,65535,0,65535,-2000,72,0,0,0x00C0,3,96,0x4982,0x0000,0x08,0x0008,0x50,0x0814,0x0038,0x0000,0x0002,0x0000,0x0000,0x0000,0x0000,0x0000,0x0000,4185,4186,8373,8074,0,0,0,0,0,28.4,-53.5,28.4,2387,1800,2779,2129,0,2388,1800,423,355,2779,2129,27.6,27.4,1000,1000,0,0,0,14,0,0,32,2448,2432,-32,-26,2,0,0,2858,2849,0,0,-32,2,3.76,3413,2448,2432,0,1647,2448,2432,16384,969,SUCCESS
    112,2022-10-28 05:42:18,448.000,0x0076,0,65535,28.3,8371,0,0,0,150,175,86,2387,2779,65535,65535,0,65535,-2000,72,0,0,0x00C0,3,96,0x4982,0x0000,0x08,0x0008,0x50,0x0814,0x0038,0x0000,0x0002,0x0000,0x0000,0x0000,0x0000,0x0000,0x0000,4185,4186,8372,8381,0,0,0,0,0,28.3,-53.5,28.3,2387,1800,2779,2129,0,2388,1800,423,355,2779,2129,27.6,27.4,1000,1000,0,0,0,14,0,0,36,2448,2432,-32,-26,2,0,0,2858,2849,0,0,-32,2,3.76,3413,2448,2432,0,1647,2448,2432,16384,969,SUCCESS
    113,2022-10-28 05:42:22,452.000,0x0076,0,65535,28.2,8371,0,0,0,150,175,86,2387,2779,65535,65535,0,65535,-2000,72,0,0,0x00C0,3,96,0x4982,0x0000,0x08,0x0008,0x50,0x0814,0x0038,0x0000,0x0002,0x0000,0x0000,0x0000,0x0000,0x0000,0x0000,4185,4186,8373,8378,0,0,0,0,0,28.2,-53.5,28.2,2387,1800,2779,2129,0,2388,1800,423,355,2779,2129,27.6,27.4,1000,1000,0,0,0,14,0,0,40,2448,2432,-32,-26,2,0,0,2858,2849,0,0,-32,2,3.76,3413,2448,2432,0,1647,2448,2432,16384,969,SUCCESS
    114,2022-10-28 05:42:26,456.000,0x0076,0,65535,28.2,8371,0,0,0,150,175,86,2387,2779,65535,65535,0,65535,-2000,72,0,0,0x00C0,3,96,0x4982,0x0000,0x08,0x0008,0x50,0x0814,0x0038,0x0000,0x0002,0x0000,0x0000,0x0000,0x0000,0x0000,0x0000,4185,4186,8373,8375,0,0,0,0,0,28.2,-53.4,28.2,2387,1800,2779,2129,0,2388,1800,423,355,2779,2129,27.6,27.4,1000,1000,0,0,0,14,0,0,44,2448,2432,-32,-26,2,0,0,2858,2849,0,0,-32,2,3.76,3413,2448,2432,0,1647,2448,2432,16384,969,SUCCESS
    115,2022-10-28 05:42:30,460.000,0x0076,0,65535,28.1,8370,0,0,0,150,175,86,2387,2779,65535,65535,0,65535,-2000,72,0,0,0x00C0,3,96,0x4982,0x0000,0x08,0x0008,0x50,0x0814,0x0038,0x0000,0x0002,0x0000,0x0000,0x0000,0x0000,0x0000,0x0000,4185,4185,8371,8376,0,0,0,0,0,28.0,-53.5,28.0,2387,1800,2779,2129,0,2388,1800,423,355,2779,2129,27.6,27.4,1000,1000,0,0,0,14,0,0,48,2448,2432,-32,-26,2,0,0,2858,2849,0,0,-32,2,3.76,3413,2448,2432,0,1647,2448,2432,16384,969,SUCCESS
    116,2022-10-28 05:42:34,464.000,0x0076,0,65535,28.0,8370,0,0,0,150,175,86,2387,2779,65535,65535,0,65535,-2000,72,0,0,0x00C0,3,96,0x4982,0x0000,0x08,0x0008,0x50,0x0814,0x0038,0x0000,0x0002,0x0000,0x0000,0x0000,0x0000,0x0000,0x0000,4185,4185,8373,8374,0,0,0,0,0,28.0,-53.4,28.0,2387,1800,2779,2129,0,2388,1800,423,355,2779,2129,27.6,27.4,1000,1000,0,0,0,14,0,0,52,2448,2432,-32,-26,2,0,0,2858,2849,0,0,-32,2,3.76,3413,2448,2432,0,1647,2448,2432,16384,969,SUCCESS
    

    软件显示是COV,不是OCC。

    LOG的数据,上位机显示的界面,万用表测试到的电压

  • 您好,由于问题比较复杂,我需要询问更了解这款芯片的TI工程师,再帮您解答,稍后回复。

  • 您好,Looking at the log file, I see the gauge is working as expected. When Charge FET turns off (due to COV), the current sensed by the gauge at BAT side immediately drops to zero. The gauge is doing what is supposed to do. Please see below

    The gauge uses Voltage sensed at V-Bat side to preform its gauging algorithm. So, I don't think this will cause any issues as for the gauging aspect. Please see below. 

    Looking at the image above, I see that V-Pack is stable until COV. At COV event, the gauge opens the CHG FET and no charging current is allowed. This is what is expected from the gauge point of view. Any measurement after COV is not relevant as the gauge will ignore this. 

    Notice how Vpack is bouncing up and down, this is the reason why your FLUKE measurement is different from what the gauge reports.

    Have you tried measuring VPACK before COV? It looks like VPACK is very stable before COV.

    I would also double check the parallel FET connections. Please read the below app notes which reference to parallel FET applications.

    https://www.ti.com/lit/an/sluaa09a/sluaa09a.pdf?ts=1666972968324&ref_url=https%253A%252F%252Fwww.ti.com%252Fproduct%252FBQ76952

    https://www.ti.com/lit/an/slva729a/slva729a.pdf?ts=1666973248359&ref_url=https%253A%252F%252Fwww.ti.com%252Fproduct%252FBQ76200