This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

BQ40Z50-R2: BQ40Z50-R4 鋰鐵Golden Learning失敗

Part Number: BQ40Z50-R2
Other Parts Discussed in Thread: BQ40Z50, BQSTUDIO

Hi 您好

FW  版本  bq40z50R4 FirmwareBundle-4.03

使用電芯 Pinyou- PYR18650  4S2P  Chem ID 4106

電芯特性是 2.5V ~ 3.6V

依照Cell 0.5C 放電 還學習

放電後靜置5小時10分    充電後靜置2小時10分 

參數RSOC 0 ~ 100% 是 2.8V  (11.2V) ~  3.5V (14V)

Golden Learning 從未更新Qmax  Ra Table .....等等

參數設定gg檔案如下

另外有2個問題

1. 也未看過平衡啟動過

2. 鋰鐵是否可用R1 OR R2 版本 這兩個版本確穩定多了

LiFePO04.gg.csv