This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

TLV61220不能稳定输出,且升压倍数与理论不符



电路按此原理图搭建,滤波电容使用了10uF电解电容101钽电容

电感自己绕制,使用LCR测量仪测试为5.4uH.

测试参数如下:       

Vin / V FB / V Vout / V Vout / Vin
 1.083 0.269  1.662 1.5
2.168 0.419 2.645 1.2
2.983 0.516 3.220 1.1

为什么输出不能稳定呢,且理论Vout / Vin =6.56,实际数据却不对,经多次检查电路连接与原理图一致。

1.请问各位老师这可能是什么原因?

2.手册说:A ceramic capacitor placed as close as possible to the VBAT and GND pins of the IC is recommended.

我没有使用陶瓷电容,且没有太接近VBAT,这是问题的原因吗?

 芯片方向肯定没错,按下图确定: