This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

BQ76952: 大电流充电时bq76952的VC1电压变低

Part Number: BQ76952

如下图设计方案,B0通过采样线直接连接BAT-,AGND通过功率回路的检流电阻(0.15mR)连接到BAT-,在大电流充电时VC1的采样电压总是会变低0.3~1.5V不等,从而触发低压相关保护。

  • 您好,请参考评估板的电路。

    www.ti.com/.../sluuc33a.pdf

  • Star 您好,设计之初就有参考评估板电路。第一节电压VC1的采样是通过和VC0的差分信号采样的吗,和VSS有没有关系?我试过将VC1、VC0的滤波电容地和952的17Pin VSS单独引线到B-,问题仍没有得到解决。

  • 您好 ,发过来的电路上没有看到VSS,和B-,还有检测电阻,能将这部分电路完整的发过来吗?

  • 当然,这部分的电路简图如下,电路图中的B0和B-都是连接到PACK的BAT- 。另外请教一下,第一节电压VC1的采样是通过和VC0的差分信号采样的吗,和VSS有没有关系?

  • 您好,问题是否仅发生在充电过程中?还是放电电流也会发生?你用的是什么电流?

    BAT-, VC0 and Vss should all be referenced to roughly the same potential reference point. So Vss should be connected to BAT-. I can see that Vss is referenced after the sense resistor, in other words to PACK-. We recommend to have VSS referenced to BAT-. We've seen issues if Vss is referenced to PACK- for some customers.

  • 目前仅在充电过程中发生此现象,充电使用的是直流源充电。我也考虑过大电流的时候可能在采样电阻上产生一个压降影响到VSS的“0”电平,但是对于采样来说VC1和VC0采用的是差分采样,两者滤波电容又是共同的参考地,共模干扰应该不会影响采样值才对。当然,对于VC0、VSS和BAT-我们后期会更改使其处于同一个参考点,只是困惑大电流充电时可以使VC1采样值变小的环路在哪里。

  • 您好,请参考下面内容

    Can they measure the voltage directly from the pins to Vss, so VC1 to Vss, VC0 to Vss, VC1 to VC0 during high charging and see if it matches the measurements by the IC. They mention they see a voltage difference between 0.3-V to 1.5-V, is this related to the amount of current? Or it varies randomly?

    At what currents do they see the issue?

    Is there any voltage drop on the traces themselves?