能否有人讲讲ucd3138和c2000系列作数字电源控制上有什么不同吗?
有朋友提到c2000做起来会灵活度高一些,可否有具体的说明?
另,ucd3138做峰值电流控制可否?有什么困难点?
This thread has been locked.
If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.
你好,UCD3138是专用的数字电源控制器,从电源系统的角度来看,它和C2000没有太大的区别。不过从芯片的角度来看,C2000确实更为灵活。UCD3138是专门针对数字电源的控制器,因此很多外围设备是专门为电源系统设计的,例如EADC,Digital Compensatior以及DPWM。这些专用的外设给电源设计带来了很大的方便,但也因此显得不够灵活了。在软开关方面,个人觉得UCD3138更有优势,在电源设计方面的潜力更大。
UCD3138采用CCS软件编写代码,但需要TI专门的数字电源软件下载(可以从TI官网下载)。目前D3138主要用于通信电源、AC-DC以及隔离的DC-DC中。
UCD3138可以很方便的实现峰值电流控制,具体内容可以参考TI数据手册中的相关章节。
开关频率在1MHz的情况,采用数字控制未必是合理的选择。数字电源的输出功率一般在数百W,开关频率在数百KHz,这主要是大功率MOSFET的特性决定的。不知道你的设计功率有多大。如果是低压小功率的,建议使用集成IC来设计。对于UCD3138本身来说,输出1MHz的PWM信号是没有问题的,内部DPWM的时钟是250M。
UCD3138的内部环路实际上是一个数字的PID,通过程序来配置各个环节的参数。环路参数可以通过GUI来计算,但仍然需要通过编写程序来完成实际的参数配置。所以内部虽然是2p2z的形式,但通过配置其实可以完成想要的补偿电路。