This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

ucd3138和c2000数字控制电源应用有何不同

Other Parts Discussed in Thread: UCD3138

     能否有人讲讲ucd3138和c2000系列作数字电源控制上有什么不同吗?

      有朋友提到c2000做起来会灵活度高一些,可否有具体的说明?

      另,ucd3138做峰值电流控制可否?有什么困难点?

  • 你好,UCD3138是专用的数字电源控制器,从电源系统的角度来看,它和C2000没有太大的区别。不过从芯片的角度来看,C2000确实更为灵活。UCD3138是专门针对数字电源的控制器,因此很多外围设备是专门为电源系统设计的,例如EADC,Digital Compensatior以及DPWM。这些专用的外设给电源设计带来了很大的方便,但也因此显得不够灵活了。在软开关方面,个人觉得UCD3138更有优势,在电源设计方面的潜力更大。

    UCD3138采用CCS软件编写代码,但需要TI专门的数字电源软件下载(可以从TI官网下载)。目前D3138主要用于通信电源、AC-DC以及隔离的DC-DC中。

    UCD3138可以很方便的实现峰值电流控制,具体内容可以参考TI数据手册中的相关章节。

  • 另外追加问一下:

    1.如果要开发一个1Mhz频率的电源,是否ucd3138会更加合适?注意到内部有250MHZ clock,应该是专门为DPWM做的吧?

    2. UCD3138对于环路的控制上,是否是一个固定的2p2z的方法?是类似于GUI的界面来做的吗,象Digital POL芯片里那样?这是否就是设计中最大的局限性。

    不好意思初步开始设计数字电源,很多还不是很了解。

  • 开关频率在1MHz的情况,采用数字控制未必是合理的选择。数字电源的输出功率一般在数百W,开关频率在数百KHz,这主要是大功率MOSFET的特性决定的。不知道你的设计功率有多大。如果是低压小功率的,建议使用集成IC来设计。对于UCD3138本身来说,输出1MHz的PWM信号是没有问题的,内部DPWM的时钟是250M。

    UCD3138的内部环路实际上是一个数字的PID,通过程序来配置各个环节的参数。环路参数可以通过GUI来计算,但仍然需要通过编写程序来完成实际的参数配置。所以内部虽然是2p2z的形式,但通过配置其实可以完成想要的补偿电路。